<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLinux...drm/bridge...sec-dsim.c driver...Tianma Display...</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-drm-bridge-sec-dsim-c-driver-Tianma-Display/m-p/1424866#M187969</link>
    <description>&lt;P&gt;Hey Folks,&lt;/P&gt;&lt;P&gt;Ken, here, please help…lol…desperate!!&lt;/P&gt;&lt;P&gt;I’m not sure what’s causing this timing problem…at least I think it is a timing issue.&lt;/P&gt;&lt;P&gt;We made some changes in sec-dsim.c, and “sec_mipi_dsim_check_pll_out” keeps getting called from “…dsim-imx.c” i.e., “printk” keeps dumping msgs to the linux console of my 8mminilpd4 evkit(2018 version/NO PCA9450)…files attached!&lt;/P&gt;&lt;P&gt;Plus, I am trying to get the attached device tree files to work. One is supposed to work with the Tianma touch display and the&lt;/P&gt;&lt;P&gt;other with a HDMI monitor. Both connect via the mipi-dsi mini-sas connector. The HDMI monitor connects via NXP&lt;/P&gt;&lt;P&gt;IMX-MIPI-HDMI accessory card and Mini-SAS cable, and the Tianma connects with a mipi-dsi mini-sas connector. I can get the Tianma&lt;/P&gt;&lt;P&gt;to connect using the attached tianma-DT file, but I can not get the hdmi monitor to connect with the attached hdmi-DT file.&amp;nbsp; In both cases, I cannot get the ov9734 camera to work. We did get the ov5640 to work, but not sure how to set up the ov9734 in linux Kconfig/Kbuild, etc.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks very much for your help!!&lt;/P&gt;&lt;P&gt;Blessings,&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;P&gt;PS...I also need to get an AR0144 camera to connect; our hardware product will select 1 of 3&lt;/P&gt;&lt;P&gt;cameras (2-ov9734 &amp;amp; 1-ar0144) via i2c mux. Do I need both types in the DT, plus the linux drivers&lt;/P&gt;&lt;P&gt;and setup in Kconfig/Kbuild…THANKS, Again!! I did find driver for a “ov9734.c”, not a “ar0144.c” in a Linux source tree…&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Mar 2022 01:55:11 GMT</pubDate>
    <dc:creator>wkb</dc:creator>
    <dc:date>2022-03-09T01:55:11Z</dc:date>
    <item>
      <title>Linux...drm/bridge...sec-dsim.c driver...Tianma Display...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-drm-bridge-sec-dsim-c-driver-Tianma-Display/m-p/1424866#M187969</link>
      <description>&lt;P&gt;Hey Folks,&lt;/P&gt;&lt;P&gt;Ken, here, please help…lol…desperate!!&lt;/P&gt;&lt;P&gt;I’m not sure what’s causing this timing problem…at least I think it is a timing issue.&lt;/P&gt;&lt;P&gt;We made some changes in sec-dsim.c, and “sec_mipi_dsim_check_pll_out” keeps getting called from “…dsim-imx.c” i.e., “printk” keeps dumping msgs to the linux console of my 8mminilpd4 evkit(2018 version/NO PCA9450)…files attached!&lt;/P&gt;&lt;P&gt;Plus, I am trying to get the attached device tree files to work. One is supposed to work with the Tianma touch display and the&lt;/P&gt;&lt;P&gt;other with a HDMI monitor. Both connect via the mipi-dsi mini-sas connector. The HDMI monitor connects via NXP&lt;/P&gt;&lt;P&gt;IMX-MIPI-HDMI accessory card and Mini-SAS cable, and the Tianma connects with a mipi-dsi mini-sas connector. I can get the Tianma&lt;/P&gt;&lt;P&gt;to connect using the attached tianma-DT file, but I can not get the hdmi monitor to connect with the attached hdmi-DT file.&amp;nbsp; In both cases, I cannot get the ov9734 camera to work. We did get the ov5640 to work, but not sure how to set up the ov9734 in linux Kconfig/Kbuild, etc.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks very much for your help!!&lt;/P&gt;&lt;P&gt;Blessings,&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;P&gt;PS...I also need to get an AR0144 camera to connect; our hardware product will select 1 of 3&lt;/P&gt;&lt;P&gt;cameras (2-ov9734 &amp;amp; 1-ar0144) via i2c mux. Do I need both types in the DT, plus the linux drivers&lt;/P&gt;&lt;P&gt;and setup in Kconfig/Kbuild…THANKS, Again!! I did find driver for a “ov9734.c”, not a “ar0144.c” in a Linux source tree…&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Mar 2022 01:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-drm-bridge-sec-dsim-c-driver-Tianma-Display/m-p/1424866#M187969</guid>
      <dc:creator>wkb</dc:creator>
      <dc:date>2022-03-09T01:55:11Z</dc:date>
    </item>
  </channel>
</rss>