<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8 Mini Power Up sequence</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8-Mini-Power-Up-sequence/m-p/1424635#M187956</link>
    <description>&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;in imx8Mini Quad Lite, if I do not use MIPI interface, is it&lt;STRONG&gt; necessary&lt;/STRONG&gt; to connect&amp;nbsp;VDD_MIPI_1P2,&amp;nbsp;VDD_MIPI_1P8 e&amp;nbsp;VDD_MIPI_0P9?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because it is written in the datasheet to leave them unconnected if they are unused, but in the power up sequence of the imx8M there are timings related to these voltages.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Elena&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 08 Mar 2022 14:46:33 GMT</pubDate>
    <dc:creator>VISINE</dc:creator>
    <dc:date>2022-03-08T14:46:33Z</dc:date>
    <item>
      <title>imx8 Mini Power Up sequence</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-Mini-Power-Up-sequence/m-p/1424635#M187956</link>
      <description>&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;in imx8Mini Quad Lite, if I do not use MIPI interface, is it&lt;STRONG&gt; necessary&lt;/STRONG&gt; to connect&amp;nbsp;VDD_MIPI_1P2,&amp;nbsp;VDD_MIPI_1P8 e&amp;nbsp;VDD_MIPI_0P9?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because it is written in the datasheet to leave them unconnected if they are unused, but in the power up sequence of the imx8M there are timings related to these voltages.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Elena&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 14:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-Mini-Power-Up-sequence/m-p/1424635#M187956</guid>
      <dc:creator>VISINE</dc:creator>
      <dc:date>2022-03-08T14:46:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 Mini Power Up sequence</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-Mini-Power-Up-sequence/m-p/1424806#M187966</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;In datasheet power up sequence list all analog 1.8V, but it is not mandatory to have it. Please refer to&amp;nbsp;Table 17. Power-up sequence&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 21:20:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-Mini-Power-Up-sequence/m-p/1424806#M187966</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-03-08T21:20:50Z</dc:date>
    </item>
  </channel>
</rss>