<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBoot iMX 8 with M7 core enabled</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8-with-M7-core-enabled/m-p/1424541#M187944</link>
    <description>&lt;P&gt;I am developing an application for the M7 core on an&amp;nbsp;MIMX8ML8CVNKZAB. I will be using IAR IDE to develop the code and Segger J-Link Plus to connect to the target.&lt;/P&gt;&lt;P&gt;I understand I need to boot the A53 core first and then enable the M7 core.&lt;/P&gt;&lt;P&gt;Is it possible to enable the M7 core without loading an M7 application? I would like to use IAR to download the code to SRAM for debugging. Once the application is working I will figure out how to save it to an SD card for automatic booting.&lt;/P&gt;&lt;P&gt;My target board is a&amp;nbsp;VAR-SOM-MX8M-PLUS. What information do I need to place in a device tree to enable the M7?&lt;/P&gt;</description>
    <pubDate>Tue, 08 Mar 2022 11:30:53 GMT</pubDate>
    <dc:creator>hoyden</dc:creator>
    <dc:date>2022-03-08T11:30:53Z</dc:date>
    <item>
      <title>Boot iMX 8 with M7 core enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8-with-M7-core-enabled/m-p/1424541#M187944</link>
      <description>&lt;P&gt;I am developing an application for the M7 core on an&amp;nbsp;MIMX8ML8CVNKZAB. I will be using IAR IDE to develop the code and Segger J-Link Plus to connect to the target.&lt;/P&gt;&lt;P&gt;I understand I need to boot the A53 core first and then enable the M7 core.&lt;/P&gt;&lt;P&gt;Is it possible to enable the M7 core without loading an M7 application? I would like to use IAR to download the code to SRAM for debugging. Once the application is working I will figure out how to save it to an SD card for automatic booting.&lt;/P&gt;&lt;P&gt;My target board is a&amp;nbsp;VAR-SOM-MX8M-PLUS. What information do I need to place in a device tree to enable the M7?&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 11:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8-with-M7-core-enabled/m-p/1424541#M187944</guid>
      <dc:creator>hoyden</dc:creator>
      <dc:date>2022-03-08T11:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: Boot iMX 8 with M7 core enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8-with-M7-core-enabled/m-p/1424783#M187963</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You may refer to the following app note:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5317.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5317.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 19:43:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8-with-M7-core-enabled/m-p/1424783#M187963</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-03-08T19:43:05Z</dc:date>
    </item>
    <item>
      <title>Re: Boot iMX 8 with M7 core enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8-with-M7-core-enabled/m-p/1425190#M188002</link>
      <description>&lt;P&gt;Thank you, Aldo. That AN looks most helpful.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Mar 2022 09:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8-with-M7-core-enabled/m-p/1425190#M188002</guid>
      <dc:creator>hoyden</dc:creator>
      <dc:date>2022-03-09T09:59:35Z</dc:date>
    </item>
  </channel>
</rss>