<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuad Motor Control Development Platform and Pe micro</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Quad-Motor-Control-Development-Platform-and-Pe-micro/m-p/1423959#M187895</link>
    <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;we are having a strange problem with the "Quad Motor Control Development Platform".&lt;BR /&gt;This platform consists of three boards (equipped with an i.MX RT1052) already developed by NXP and the management software also developed by NXP to allow the control of up to four brushless motors.&lt;BR /&gt;The problem that until now we have not been able to solve is debugging the application with PE micro, it seems that it cannot load the application or it loads it partially or incorrectly.&lt;BR /&gt;It all works using LPC Link2 but not Pe micro.&lt;BR /&gt;Pe micro works correctly on EVKBs (with 1052 on board)!&lt;BR /&gt;The big difference between the 2 evaluations is this:&lt;BR /&gt;1) EVKB defaults to Hyper Flash&lt;BR /&gt;2) Quad motor goes on quad SPI&lt;BR /&gt;Has anyone faced similar problems?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
    <pubDate>Mon, 07 Mar 2022 14:00:41 GMT</pubDate>
    <dc:creator>gianpiero_lenta</dc:creator>
    <dc:date>2022-03-07T14:00:41Z</dc:date>
    <item>
      <title>Quad Motor Control Development Platform and Pe micro</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-Motor-Control-Development-Platform-and-Pe-micro/m-p/1423959#M187895</link>
      <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;we are having a strange problem with the "Quad Motor Control Development Platform".&lt;BR /&gt;This platform consists of three boards (equipped with an i.MX RT1052) already developed by NXP and the management software also developed by NXP to allow the control of up to four brushless motors.&lt;BR /&gt;The problem that until now we have not been able to solve is debugging the application with PE micro, it seems that it cannot load the application or it loads it partially or incorrectly.&lt;BR /&gt;It all works using LPC Link2 but not Pe micro.&lt;BR /&gt;Pe micro works correctly on EVKBs (with 1052 on board)!&lt;BR /&gt;The big difference between the 2 evaluations is this:&lt;BR /&gt;1) EVKB defaults to Hyper Flash&lt;BR /&gt;2) Quad motor goes on quad SPI&lt;BR /&gt;Has anyone faced similar problems?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 14:00:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-Motor-Control-Development-Platform-and-Pe-micro/m-p/1423959#M187895</guid>
      <dc:creator>gianpiero_lenta</dc:creator>
      <dc:date>2022-03-07T14:00:41Z</dc:date>
    </item>
  </channel>
</rss>