<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issue with LAN8720A with IMX8MN in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1418701#M187437</link>
    <description>&lt;P&gt;Please check the signals on the PHY are proper or not. e.g. the reset_n, the clock signal.&lt;/P&gt;
&lt;P&gt;Please refer to the i.MX8MNRM Table 11-78. ENET External Signals.&lt;/P&gt;</description>
    <pubDate>Thu, 24 Feb 2022 02:35:48 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2022-02-24T02:35:48Z</dc:date>
    <item>
      <title>Issue with LAN8720A with IMX8MN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1410393#M186762</link>
      <description>&lt;P&gt;Dear All,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing issue in "interfacing the LAN8720A with IMX8MN with Android 10 build". Below are the descriptions:&lt;/P&gt;&lt;P&gt;dtsi changes:&lt;/P&gt;&lt;P&gt;&amp;amp;fec1 {&lt;BR /&gt;pinctrl-names = "default";&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_fec1&amp;gt;;&lt;BR /&gt;phy-mode = "rmii";&lt;BR /&gt;phy-handle = &amp;lt;&amp;amp;ethphy0&amp;gt;;&lt;BR /&gt;fsl,magic-packet;&lt;BR /&gt;phy-reset-gpios = &amp;lt;&amp;amp;gpio5 4 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt;phy-reset-duration = &amp;lt;25&amp;gt;;&lt;BR /&gt;phy-reset-active-high;&lt;BR /&gt;//phy-supply = &amp;lt;&amp;amp;reg_3v3_p&amp;gt;;&lt;BR /&gt;status = "okay";&lt;/P&gt;&lt;P&gt;mdio {&lt;BR /&gt;#address-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt;#size-cells = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;ethphy0: ethernet-phy@0{&lt;BR /&gt;compatible = "ethernet-phy-ieee802.3-c22";&lt;BR /&gt;reg = &amp;lt;0&amp;gt;;&lt;BR /&gt;//smsc,disable-energy-detect;&lt;BR /&gt;//reset-gpios = &amp;lt;&amp;amp;gpio5 4 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt;//reset-assert-us = &amp;lt;12000&amp;gt;;&lt;BR /&gt;//reset-deassert-us = &amp;lt;13000&amp;gt;;&lt;BR /&gt;max-speed = &amp;lt;100&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pin MUX:&lt;/P&gt;&lt;P&gt;pinctrl_fec1: fec1grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX8MN_IOMUXC_ENET_MDC_ENET1_MDC 0x3 /* ENET_MDC */&lt;BR /&gt;MX8MN_IOMUXC_ENET_MDIO_ENET1_MDIO 0x23 /* ENET_MDIO */&lt;BR /&gt;MX8MN_IOMUXC_ENET_TD2_ENET1_TX_CLK 0x4000001f /* ENET_TX_CLK */&lt;BR /&gt;MX8MN_IOMUXC_ENET_TD1_ENET1_RGMII_TD1 0x56 /* ENET_TXD1 */&lt;BR /&gt;MX8MN_IOMUXC_ENET_TD0_ENET1_RGMII_TD0 0x56 /* ENET_TXD0 */&lt;BR /&gt;MX8MN_IOMUXC_ENET_RD1_ENET1_RGMII_RD1 0x56 /* ENET_RXD1 */&lt;BR /&gt;MX8MN_IOMUXC_ENET_RD0_ENET1_RGMII_RD0 0x56 /* ENET_RXD0 */&lt;BR /&gt;MX8MN_IOMUXC_ENET_RXC_ENET1_RX_ER 0x56 /* ENET_RXERR */&lt;BR /&gt;MX8MN_IOMUXC_ENET_RX_CTL_ENET1_RGMII_RX_CTL 0x56 /* ENET_CRS_DV */&lt;BR /&gt;MX8MN_IOMUXC_ENET_TX_CTL_ENET1_RGMII_TX_CTL 0x56 /* ENET_TX_EN */&lt;BR /&gt;MX8MN_IOMUXC_SPDIF_RX_GPIO5_IO4 0x41 /* ENET1_nRST */&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;I have attached the screenshot of the schematic.&lt;/P&gt;&lt;P&gt;Below is the error log:&lt;/P&gt;&lt;P&gt;8.196838] ##################### msec = 25 #######################&lt;BR /&gt;[ 8.237584] pps pps0: new PPS source ptp0&lt;BR /&gt;[ 8.248334] fec 30be0000.ethernet: Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;[ 8.255199] fec 30be0000.ethernet: Using random MAC address: 66:3d:6c:a1:91:cd&lt;BR /&gt;[ 8.263446] libphy: fec_enet_mii_bus: probed&lt;BR /&gt;[ 8.267737] Child is a phy ########################&lt;BR /&gt;[ 8.272624] ############### In else ####################&lt;BR /&gt;[ 8.278150] failed in IS_ERR ##########################&lt;BR /&gt;[ 8.283508] mdio_bus 30be0000.ethernet-1: MDIO device at address 0 is missing.&lt;BR /&gt;[ 8.291473] fec 30be0000.ethernet eth0: registered PHC device 0&lt;BR /&gt;[ 8.299761] imx-spdif sound-spdif: ASoC: failed to init link S/PDIF PCM: -517&lt;BR /&gt;[ 8.307720] sdhci-esdhc-imx 30b40000.mmc: allocated mmc-pwrseq&lt;BR /&gt;[ 8.347031] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA&lt;/P&gt;&lt;P&gt;Let me know if you need more information and your early help shall be greatly appreciated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sunil&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Feb 2022 15:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1410393#M186762</guid>
      <dc:creator>sunil_embex</dc:creator>
      <dc:date>2022-02-08T15:54:12Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LAN8720A with IMX8MN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1413742#M187019</link>
      <description>&lt;P&gt;I got the etho but not getting the ip address:&lt;/P&gt;&lt;P&gt;lo Link encap:Local Loopback&lt;BR /&gt;inet addr:127.0.0.1 Mask:255.0.0.0&lt;BR /&gt;inet6 addr: ::1/128 Scope: Host&lt;BR /&gt;UP LOOPBACK RUNNING MTU:65536 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 TX bytes:0&lt;/P&gt;&lt;P&gt;dummy0 Link encap:Ethernet HWaddr 7e:d0:da:e4:05:3f&lt;BR /&gt;inet6 addr: fe80::7cd0:daff:fee4:53f/64 Scope: Link&lt;BR /&gt;UP BROADCAST RUNNING NOARP MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:8 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 TX bytes:560&lt;/P&gt;&lt;P&gt;eth0 Link encap:Ethernet HWaddr 12:0b:86:4c:4d:b3 Driver fec&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 TX bytes:0&lt;/P&gt;&lt;P&gt;Seems there is no dhcp so can you please help what is the issue.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sunil&lt;/P&gt;</description>
      <pubDate>Tue, 15 Feb 2022 13:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1413742#M187019</guid>
      <dc:creator>sunil_embex</dc:creator>
      <dc:date>2022-02-15T13:43:52Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LAN8720A with IMX8MN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1416299#M187225</link>
      <description>&lt;P&gt;So, the PHY is working now? Did you try using ifconfig to setup an ip address?&lt;/P&gt;</description>
      <pubDate>Sun, 20 Feb 2022 06:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1416299#M187225</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-02-20T06:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LAN8720A with IMX8MN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1416358#M187236</link>
      <description>&lt;P&gt;I am able to assign but seems link is not working because my laptop is not detecting this static connection.&lt;/P&gt;&lt;P&gt;Can you please help me to confirm the following dtsi changes whether its ok or not:&lt;/P&gt;&lt;P&gt;&amp;amp;fec1 {&lt;BR /&gt;pinctrl-names = "default";&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_fec1&amp;gt;;&lt;BR /&gt;phy-mode = "rmii";&lt;BR /&gt;phy-handle = &amp;lt;&amp;amp;ethphy0&amp;gt;;&lt;BR /&gt;fsl,magic-packet;&lt;BR /&gt;phy-reset-gpios = &amp;lt;&amp;amp;gpio5 4 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt;phy-reset-duration = &amp;lt;25&amp;gt;;&lt;BR /&gt;phy-reset-active-high;&lt;BR /&gt;//phy-supply = &amp;lt;&amp;amp;reg_3v3_p&amp;gt;;&lt;BR /&gt;status = "okay";&lt;/P&gt;&lt;P&gt;mdio {&lt;BR /&gt;#address-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt;#size-cells = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;ethphy0: ethernet-phy@0{&lt;BR /&gt;compatible = "ethernet-phy-ieee802.3-c22";&lt;BR /&gt;reg = &amp;lt;0&amp;gt;;&lt;BR /&gt;//smsc,disable-energy-detect;&lt;BR /&gt;//reset-gpios = &amp;lt;&amp;amp;gpio5 4 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt;//reset-assert-us = &amp;lt;12000&amp;gt;;&lt;BR /&gt;//reset-deassert-us = &amp;lt;13000&amp;gt;;&lt;BR /&gt;max-speed = &amp;lt;100&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pin MUX:&lt;/P&gt;&lt;P&gt;pinctrl_fec1: fec1grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX8MN_IOMUXC_ENET_MDC_ENET1_MDC 0x3 /* ENET_MDC */&lt;BR /&gt;MX8MN_IOMUXC_ENET_MDIO_ENET1_MDIO 0x23 /* ENET_MDIO */&lt;BR /&gt;MX8MN_IOMUXC_ENET_TD2_ENET1_TX_CLK 0x4000001f /* ENET_TX_CLK */&lt;BR /&gt;MX8MN_IOMUXC_ENET_TD1_ENET1_RGMII_TD1 0x56 /* ENET_TXD1 */&lt;BR /&gt;MX8MN_IOMUXC_ENET_TD0_ENET1_RGMII_TD0 0x56 /* ENET_TXD0 */&lt;BR /&gt;MX8MN_IOMUXC_ENET_RD1_ENET1_RGMII_RD1 0x56 /* ENET_RXD1 */&lt;BR /&gt;MX8MN_IOMUXC_ENET_RD0_ENET1_RGMII_RD0 0x56 /* ENET_RXD0 */&lt;BR /&gt;MX8MN_IOMUXC_ENET_RXC_ENET1_RX_ER 0x56 /* ENET_RXERR */&lt;BR /&gt;MX8MN_IOMUXC_ENET_RX_CTL_ENET1_RGMII_RX_CTL 0x56 /* ENET_CRS_DV */&lt;BR /&gt;MX8MN_IOMUXC_ENET_TX_CTL_ENET1_RGMII_TX_CTL 0x56 /* ENET_TX_EN */&lt;BR /&gt;MX8MN_IOMUXC_SPDIF_RX_GPIO5_IO4 0x41 /* ENET1_nRST */&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Added Support of 50Mhz which was missing before in imx8mn.dtsi&lt;/P&gt;&lt;P&gt;&amp;lt;&amp;amp;clk IMX8MN_SYS_PLL2_125M&amp;gt;,&lt;BR /&gt;+ &amp;lt;&amp;amp;clk IMX8MN_SYS_PLL2_50M&amp;gt;;&lt;BR /&gt;+ assigned-clock-rates = &amp;lt;0&amp;gt;, &amp;lt;50000000&amp;gt;,&amp;lt;100000000&amp;gt; &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;Please confirm the dtsi changes and I have also attached the schematic.&lt;/P&gt;&lt;P&gt;Your early help will be greatly appriciated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sunil&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Feb 2022 02:08:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1416358#M187236</guid>
      <dc:creator>sunil_embex</dc:creator>
      <dc:date>2022-02-21T02:08:01Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LAN8720A with IMX8MN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1418701#M187437</link>
      <description>&lt;P&gt;Please check the signals on the PHY are proper or not. e.g. the reset_n, the clock signal.&lt;/P&gt;
&lt;P&gt;Please refer to the i.MX8MNRM Table 11-78. ENET External Signals.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 02:35:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1418701#M187437</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-02-24T02:35:48Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LAN8720A with IMX8MN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1422670#M187754</link>
      <description>&lt;P&gt;Hi Jummychan,&lt;/P&gt;&lt;P&gt;Still Phy is not working. I have attached the waveform screenshot of MDIO,MDC.. pins.&lt;/P&gt;&lt;P&gt;Can you please also check whether the settings are ok or not&amp;nbsp; which I have used in dts.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sunil&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Mar 2022 12:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-LAN8720A-with-IMX8MN/m-p/1422670#M187754</guid>
      <dc:creator>sunil_embex</dc:creator>
      <dc:date>2022-03-03T12:17:10Z</dc:date>
    </item>
  </channel>
</rss>