<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Serial Download using USB micro AB connectors on iMX8ML (iMX8MPlus)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-using-USB-micro-AB-connectors-on-iMX8ML/m-p/1417282#M187317</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191259"&gt;@swapnilturambekar&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; i.MX boot ROM in (USB) serial downloader mode configures&lt;BR /&gt;i.MX USB port as a HID devices. USB3 (/ C) is not supported at this&lt;BR /&gt;stage. Under UUU, i.MX boot ROM is used only to download u-boot.imx&lt;BR /&gt;via HID device, then the following configuring is a prerogative of&lt;BR /&gt;U-boot. Customers can adapt (UUU) U-boot as needed.&lt;BR /&gt;&lt;BR /&gt;Also it is possible to use TFTP under U-boot &lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Feb 2022 07:41:14 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2022-02-22T07:41:14Z</dc:date>
    <item>
      <title>Serial Download using USB micro AB connectors on iMX8ML (iMX8MPlus)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-using-USB-micro-AB-connectors-on-iMX8ML/m-p/1415074#M187109</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to flash iMX8ML processor (using&amp;nbsp;imx8mp-lpddr4-evk.conf file) in custom board. Is my configuration file correct to flash iMX8ML processor? In the custom board I am using Micro AB USB connector. We are trying to flash using usb1 port. but after bootloader the flashing process stucked.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What changes I have to made to flash using micro AB USB connector.? Please suggest. I have attached the log for the same. can someone please guide here to flash the board.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Feb 2022 07:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-using-USB-micro-AB-connectors-on-iMX8ML/m-p/1415074#M187109</guid>
      <dc:creator>swapnilturambekar</dc:creator>
      <dc:date>2022-02-17T07:50:53Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Download using USB micro AB connectors on iMX8ML (iMX8MPlus)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-using-USB-micro-AB-connectors-on-iMX8ML/m-p/1417282#M187317</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191259"&gt;@swapnilturambekar&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; i.MX boot ROM in (USB) serial downloader mode configures&lt;BR /&gt;i.MX USB port as a HID devices. USB3 (/ C) is not supported at this&lt;BR /&gt;stage. Under UUU, i.MX boot ROM is used only to download u-boot.imx&lt;BR /&gt;via HID device, then the following configuring is a prerogative of&lt;BR /&gt;U-boot. Customers can adapt (UUU) U-boot as needed.&lt;BR /&gt;&lt;BR /&gt;Also it is possible to use TFTP under U-boot &lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 07:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-using-USB-micro-AB-connectors-on-iMX8ML/m-p/1417282#M187317</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2022-02-22T07:41:14Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Download using USB micro AB connectors on iMX8ML (iMX8MPlus)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-using-USB-micro-AB-connectors-on-iMX8ML/m-p/1419130#M187472</link>
      <description>&lt;P&gt;It is very clear debug log information the custom board has no typeC chip different from the i.MX8MP evk.&lt;/P&gt;
&lt;P&gt;The NXP bsp release is design for the i.MX8MP evk board, which has typeC chip.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please remove the typeC configuration in uboot configuration file.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;if the custom board has no usb id pin as otg, you can&amp;nbsp;use the dr_mode with "peripheral" in dts.&lt;/P&gt;
&lt;P&gt;And finished the necessary modification according to the custom board hardware design.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;DRAM: 6 GiB&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-19&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 13:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-using-USB-micro-AB-connectors-on-iMX8ML/m-p/1419130#M187472</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2022-02-24T13:57:35Z</dc:date>
    </item>
  </channel>
</rss>