<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBoot From NAND not supporting with 2.6.35 Kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-From-NAND-not-supporting-with-2-6-35-Kernel/m-p/235952#M18716</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Boot From NAND not supporting with 2.6.35 Kernel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When Im using the kernel 2.6.31 Icould easily boot from either SD Card or the NAND Flash , i.e followed the same procedure of freescale to copy the kernel and Filesystem to NAND using ubifs with the LTIB command line as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;noinitrd console=ttyAM0,115200 ubi.mtd=1 root=ubi0:rootfs0 rootfstype=ubifs rw gpmi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when trying to the same with kernel 2.6.35 , there is a kernel panic as shown below?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: irq 11, io base 0x80080000 &lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00 &lt;/P&gt;&lt;P&gt;hub 1-0:1.0: USB hub found &lt;/P&gt;&lt;P&gt;hub 1-0:1.0: 1 port detected &lt;/P&gt;&lt;P&gt;Initializing USB Mass Storage driver... &lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage &lt;/P&gt;&lt;P&gt;USB Mass Storage support registered. &lt;/P&gt;&lt;P&gt;ARC USBOTG Device Controller driver (1 August 2005) &lt;/P&gt;&lt;P&gt;udc: request mem region for fsl-usb2-udc failed &lt;/P&gt;&lt;P&gt;fsl-usb2-udc: probe of fsl-usb2-udc failed with error -16 &lt;/P&gt;&lt;P&gt;mice: PS/2 mouse device common for all mice &lt;/P&gt;&lt;P&gt;input: mxs-kbd as /class/input/input0 &lt;/P&gt;&lt;P&gt;input: MXS touchscreen as /class/input/input1 &lt;/P&gt;&lt;P&gt;MXS RTC driver v1.0 hardware v2.0.0 &lt;/P&gt;&lt;P&gt;mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0 &lt;/P&gt;&lt;P&gt;i2c /dev entries driver &lt;/P&gt;&lt;P&gt;IR NEC protocol handler initialized &lt;/P&gt;&lt;P&gt;IR RC5(x) protocol handler initialized &lt;/P&gt;&lt;P&gt;IR RC6 protocol handler initialized &lt;/P&gt;&lt;P&gt;IR JVC protocol handler initialized &lt;/P&gt;&lt;P&gt;IR Sony protocol handler initialized &lt;/P&gt;&lt;P&gt;Linux video capture interface: v2.00 &lt;/P&gt;&lt;P&gt;mxs-pxp mxs-pxp.0: initialized &lt;/P&gt;&lt;P&gt;mxs watchdog: initialized, heartbeat 19 sec &lt;/P&gt;&lt;P&gt;mxs-mmc: MXS SSP Controller MMC Interface driver &lt;/P&gt;&lt;P&gt;mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 14 ERRIRQ 15 &lt;/P&gt;&lt;P&gt;dcp dcp.0: DCP crypto enabled.! &lt;/P&gt;&lt;P&gt;mxs-adc-audio mxs-adc-audio.0: MXS ADC/DAC Audio Codec &lt;/P&gt;&lt;P&gt;No device for DAI mxs adc/dac &lt;/P&gt;&lt;P&gt;No device for DAI mxs adc/dac &lt;/P&gt;&lt;P&gt;asoc: mxs adc/dac &amp;lt;-&amp;gt; mxs adc/dac mapping ok &lt;/P&gt;&lt;P&gt;asoc: failed to init MXS ADC/DAC &lt;/P&gt;&lt;P&gt;ALSA device list: &lt;/P&gt;&lt;P&gt;&amp;nbsp; #0: MXS EVK (mxs adc/dac) &lt;/P&gt;&lt;P&gt;TCP cubic registered &lt;/P&gt;&lt;P&gt;NET: Registered protocol family 10 &lt;/P&gt;&lt;P&gt;IPv6 over IPv4 tunneling driver &lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17 &lt;/P&gt;&lt;P&gt;mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:00:37 UTC (37) &lt;/P&gt;&lt;P&gt;UBIFS error (pid 1): ubifs_get_sb: cannot open "ubi0:rootfs0", error -19 &lt;/P&gt;&lt;P&gt;VFS: Cannot open root device "ubi0:rootfs0" or unknown-block(0,0) &lt;/P&gt;&lt;P&gt;Please append a correct "root=" boot option; here are the available partitions: &lt;/P&gt;&lt;P&gt;1f00&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40960 mtdblock0 (driver?) &lt;/P&gt;&lt;P&gt;1f01 4153344 mtdblock1 (driver?) &lt;/P&gt;&lt;P&gt;1f02 2097152 mtdblock2 (driver?) &lt;/P&gt;&lt;P&gt;1f03 2056192 mtdblock3 (driver?) &lt;/P&gt;&lt;P&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can somebody help me in the bootable procedure to copy the kernel and filesystem to NAND ? Please let me know if any changes are also required with the configurations other than that are mentioned in the reference manual? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Sep 2013 05:56:55 GMT</pubDate>
    <dc:creator>Nagraj</dc:creator>
    <dc:date>2013-09-17T05:56:55Z</dc:date>
    <item>
      <title>Boot From NAND not supporting with 2.6.35 Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-From-NAND-not-supporting-with-2-6-35-Kernel/m-p/235952#M18716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Boot From NAND not supporting with 2.6.35 Kernel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When Im using the kernel 2.6.31 Icould easily boot from either SD Card or the NAND Flash , i.e followed the same procedure of freescale to copy the kernel and Filesystem to NAND using ubifs with the LTIB command line as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;noinitrd console=ttyAM0,115200 ubi.mtd=1 root=ubi0:rootfs0 rootfstype=ubifs rw gpmi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when trying to the same with kernel 2.6.35 , there is a kernel panic as shown below?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: irq 11, io base 0x80080000 &lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00 &lt;/P&gt;&lt;P&gt;hub 1-0:1.0: USB hub found &lt;/P&gt;&lt;P&gt;hub 1-0:1.0: 1 port detected &lt;/P&gt;&lt;P&gt;Initializing USB Mass Storage driver... &lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage &lt;/P&gt;&lt;P&gt;USB Mass Storage support registered. &lt;/P&gt;&lt;P&gt;ARC USBOTG Device Controller driver (1 August 2005) &lt;/P&gt;&lt;P&gt;udc: request mem region for fsl-usb2-udc failed &lt;/P&gt;&lt;P&gt;fsl-usb2-udc: probe of fsl-usb2-udc failed with error -16 &lt;/P&gt;&lt;P&gt;mice: PS/2 mouse device common for all mice &lt;/P&gt;&lt;P&gt;input: mxs-kbd as /class/input/input0 &lt;/P&gt;&lt;P&gt;input: MXS touchscreen as /class/input/input1 &lt;/P&gt;&lt;P&gt;MXS RTC driver v1.0 hardware v2.0.0 &lt;/P&gt;&lt;P&gt;mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0 &lt;/P&gt;&lt;P&gt;i2c /dev entries driver &lt;/P&gt;&lt;P&gt;IR NEC protocol handler initialized &lt;/P&gt;&lt;P&gt;IR RC5(x) protocol handler initialized &lt;/P&gt;&lt;P&gt;IR RC6 protocol handler initialized &lt;/P&gt;&lt;P&gt;IR JVC protocol handler initialized &lt;/P&gt;&lt;P&gt;IR Sony protocol handler initialized &lt;/P&gt;&lt;P&gt;Linux video capture interface: v2.00 &lt;/P&gt;&lt;P&gt;mxs-pxp mxs-pxp.0: initialized &lt;/P&gt;&lt;P&gt;mxs watchdog: initialized, heartbeat 19 sec &lt;/P&gt;&lt;P&gt;mxs-mmc: MXS SSP Controller MMC Interface driver &lt;/P&gt;&lt;P&gt;mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 14 ERRIRQ 15 &lt;/P&gt;&lt;P&gt;dcp dcp.0: DCP crypto enabled.! &lt;/P&gt;&lt;P&gt;mxs-adc-audio mxs-adc-audio.0: MXS ADC/DAC Audio Codec &lt;/P&gt;&lt;P&gt;No device for DAI mxs adc/dac &lt;/P&gt;&lt;P&gt;No device for DAI mxs adc/dac &lt;/P&gt;&lt;P&gt;asoc: mxs adc/dac &amp;lt;-&amp;gt; mxs adc/dac mapping ok &lt;/P&gt;&lt;P&gt;asoc: failed to init MXS ADC/DAC &lt;/P&gt;&lt;P&gt;ALSA device list: &lt;/P&gt;&lt;P&gt;&amp;nbsp; #0: MXS EVK (mxs adc/dac) &lt;/P&gt;&lt;P&gt;TCP cubic registered &lt;/P&gt;&lt;P&gt;NET: Registered protocol family 10 &lt;/P&gt;&lt;P&gt;IPv6 over IPv4 tunneling driver &lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17 &lt;/P&gt;&lt;P&gt;mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:00:37 UTC (37) &lt;/P&gt;&lt;P&gt;UBIFS error (pid 1): ubifs_get_sb: cannot open "ubi0:rootfs0", error -19 &lt;/P&gt;&lt;P&gt;VFS: Cannot open root device "ubi0:rootfs0" or unknown-block(0,0) &lt;/P&gt;&lt;P&gt;Please append a correct "root=" boot option; here are the available partitions: &lt;/P&gt;&lt;P&gt;1f00&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40960 mtdblock0 (driver?) &lt;/P&gt;&lt;P&gt;1f01 4153344 mtdblock1 (driver?) &lt;/P&gt;&lt;P&gt;1f02 2097152 mtdblock2 (driver?) &lt;/P&gt;&lt;P&gt;1f03 2056192 mtdblock3 (driver?) &lt;/P&gt;&lt;P&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can somebody help me in the bootable procedure to copy the kernel and filesystem to NAND ? Please let me know if any changes are also required with the configurations other than that are mentioned in the reference manual? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2013 05:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-From-NAND-not-supporting-with-2-6-35-Kernel/m-p/235952#M18716</guid>
      <dc:creator>Nagraj</dc:creator>
      <dc:date>2013-09-17T05:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: Boot From NAND not supporting with 2.6.35 Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-From-NAND-not-supporting-with-2-6-35-Kernel/m-p/235953#M18717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Some instructions for ubifs are here: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/254021"&gt;https://community.freescale.com/thread/254021&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might be missing "rootwait" parameter in kernel command line.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2013 07:40:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-From-NAND-not-supporting-with-2-6-35-Kernel/m-p/235953#M18717</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2013-09-17T07:40:49Z</dc:date>
    </item>
  </channel>
</rss>