<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic tamper pin IMX6Q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/tamper-pin-IMX6Q/m-p/1414495#M187064</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we're using an iMX6Dual based board with linux 5.4.129 and we'd like to enable&lt;BR /&gt;tamper detection on pad TAMPER (signal SNVS_TAMPER).&lt;/P&gt;&lt;P&gt;Looking into the driver linux/drivers/crypto/caam/secvio.c it seems to us that&lt;BR /&gt;LP registers are never touched... so we're puzzled to know how the&lt;BR /&gt;"external-pin-tamper" in the driver should take effect!&lt;/P&gt;&lt;P&gt;Is this the right driver to use or we needed something different? We move the&lt;BR /&gt;signal on pad TAMPER but no IRQs arrive....&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;</description>
    <pubDate>Wed, 16 Feb 2022 13:48:38 GMT</pubDate>
    <dc:creator>marcomaioli</dc:creator>
    <dc:date>2022-02-16T13:48:38Z</dc:date>
    <item>
      <title>tamper pin IMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/tamper-pin-IMX6Q/m-p/1414495#M187064</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we're using an iMX6Dual based board with linux 5.4.129 and we'd like to enable&lt;BR /&gt;tamper detection on pad TAMPER (signal SNVS_TAMPER).&lt;/P&gt;&lt;P&gt;Looking into the driver linux/drivers/crypto/caam/secvio.c it seems to us that&lt;BR /&gt;LP registers are never touched... so we're puzzled to know how the&lt;BR /&gt;"external-pin-tamper" in the driver should take effect!&lt;/P&gt;&lt;P&gt;Is this the right driver to use or we needed something different? We move the&lt;BR /&gt;signal on pad TAMPER but no IRQs arrive....&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 13:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/tamper-pin-IMX6Q/m-p/1414495#M187064</guid>
      <dc:creator>marcomaioli</dc:creator>
      <dc:date>2022-02-16T13:48:38Z</dc:date>
    </item>
    <item>
      <title>Re: tamper pin IMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/tamper-pin-IMX6Q/m-p/1416750#M187276</link>
      <description>&lt;P&gt;The external tamper functionality is not implemented&amp;nbsp;in the Linux BSP for i.MX6Dual/Quad processor.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Mon, 21 Feb 2022 11:42:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/tamper-pin-IMX6Q/m-p/1416750#M187276</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2022-02-21T11:42:59Z</dc:date>
    </item>
  </channel>
</rss>