<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: NXP i.MX8M Mini System kernel panic in Yocto 2.5.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX8M-Mini-System-kernel-panic-in-Yocto-2-5/m-p/1413877#M187031</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;By the error it is a failed read access, more information about this can be found in the D3.5 ARMv8 Architecture Reference Manual.&lt;BR /&gt;&lt;BR /&gt;It may be useful to look into the following commit:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.10.y&amp;amp;id=677fe555cbfb188af58cce105f4dae9505e58c31" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.10.y&amp;amp;id=677fe555cbfb188af58cce105f4dae9505e58c31&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Also, would it be possible to try with a more recent kernel release?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Tue, 15 Feb 2022 19:51:18 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-02-15T19:51:18Z</dc:date>
    <item>
      <title>NXP i.MX8M Mini System kernel panic in Yocto 2.5.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX8M-Mini-System-kernel-panic-in-Yocto-2-5/m-p/1405828#M186377</link>
      <description>&lt;P&gt;Hi NXP&amp;nbsp;&lt;/P&gt;&lt;P&gt;Our customer use the i.MX8M Mini solution. (Yocto 2.5)&lt;/P&gt;&lt;P&gt;He try modify and add rs-485 application.&lt;/P&gt;&lt;P&gt;**&amp;nbsp;drivers/tty/serial/imx.c **&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;-#define RXTL_UART 16 /* For uart */&lt;BR /&gt;+#define RXTL_UART 4 /* For uart */&lt;/P&gt;&lt;P&gt;He run the application, then debug message show "kernel panic".&lt;/P&gt;&lt;P&gt;Please check the modify patch. (0001_tsl_kernel_modify.patch) and System Crash_info.txt&amp;nbsp;&lt;/P&gt;&lt;P&gt;Our customer try modify the RXTL_UART&amp;nbsp; 4 (in driver/tty/serial/imx.c)&lt;/P&gt;&lt;P&gt;Do you have any advice about fixed the kernel panic issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jan 2022 07:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX8M-Mini-System-kernel-panic-in-Yocto-2-5/m-p/1405828#M186377</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2022-01-27T07:53:42Z</dc:date>
    </item>
    <item>
      <title>Re: NXP i.MX8M Mini System kernel panic in Yocto 2.5.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX8M-Mini-System-kernel-panic-in-Yocto-2-5/m-p/1413877#M187031</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;By the error it is a failed read access, more information about this can be found in the D3.5 ARMv8 Architecture Reference Manual.&lt;BR /&gt;&lt;BR /&gt;It may be useful to look into the following commit:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.10.y&amp;amp;id=677fe555cbfb188af58cce105f4dae9505e58c31" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.10.y&amp;amp;id=677fe555cbfb188af58cce105f4dae9505e58c31&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Also, would it be possible to try with a more recent kernel release?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Feb 2022 19:51:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX8M-Mini-System-kernel-panic-in-Yocto-2-5/m-p/1413877#M187031</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-02-15T19:51:18Z</dc:date>
    </item>
  </channel>
</rss>