<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQSPI vs eCSPI differences in features (i.mx 8m plus)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-vs-eCSPI-differences-in-features-i-mx-8m-plus/m-p/1412737#M186944</link>
    <description>&lt;P&gt;Is there a basic overview that shows the differences between the QuadSPI vs the eCSPI&amp;nbsp;peripherals?&lt;/P&gt;&lt;P&gt;i.e. what features and hw formats are supported, standard full duplex SPI vs half duplex when running quad, etc.&lt;/P&gt;&lt;P&gt;I have the QSPI normally used for booting the i.mx free and will instead use it to bridge to another mcu. The question is what would be the most efficient way to get a full dma'ed 2-way link between the two.&lt;/P&gt;</description>
    <pubDate>Sun, 13 Feb 2022 23:07:13 GMT</pubDate>
    <dc:creator>dav1</dc:creator>
    <dc:date>2022-02-13T23:07:13Z</dc:date>
    <item>
      <title>QSPI vs eCSPI differences in features (i.mx 8m plus)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-vs-eCSPI-differences-in-features-i-mx-8m-plus/m-p/1412737#M186944</link>
      <description>&lt;P&gt;Is there a basic overview that shows the differences between the QuadSPI vs the eCSPI&amp;nbsp;peripherals?&lt;/P&gt;&lt;P&gt;i.e. what features and hw formats are supported, standard full duplex SPI vs half duplex when running quad, etc.&lt;/P&gt;&lt;P&gt;I have the QSPI normally used for booting the i.mx free and will instead use it to bridge to another mcu. The question is what would be the most efficient way to get a full dma'ed 2-way link between the two.&lt;/P&gt;</description>
      <pubDate>Sun, 13 Feb 2022 23:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-vs-eCSPI-differences-in-features-i-mx-8m-plus/m-p/1412737#M186944</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2022-02-13T23:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI vs eCSPI differences in features (i.mx 8m plus)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-vs-eCSPI-differences-in-features-i-mx-8m-plus/m-p/1415623#M187162</link>
      <description>&lt;P&gt;Hello, &lt;BR /&gt;&lt;BR /&gt;For this you may refer to their respective chapter in the Reference manual:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MPRM" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=IMX8MPRM&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;10.1 Enhanced Configurable SPI (ECSPI)&lt;/P&gt;
&lt;P&gt;10.2 FlexSPI Controller (FlexSPI)&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Feb 2022 01:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-vs-eCSPI-differences-in-features-i-mx-8m-plus/m-p/1415623#M187162</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-02-18T01:16:53Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI vs eCSPI differences in features (i.mx 8m plus)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-vs-eCSPI-differences-in-features-i-mx-8m-plus/m-p/1434411#M188645</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Aldo,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Can you please help guide how to setup so that the DMA transfer can be triggered autonomously from either side (device spi talking upstream to the host spi == imx)&lt;/P&gt;&lt;P&gt;I was thinking a GPIO -&amp;gt; IRQ to trigger it, but would be even better if there are mechanisms as part of the FlexSPI or ECSPI peripherals themselves.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 26 Mar 2022 12:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-vs-eCSPI-differences-in-features-i-mx-8m-plus/m-p/1434411#M188645</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2022-03-26T12:00:04Z</dc:date>
    </item>
  </channel>
</rss>