<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: can't configure format on node using media-ctl</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/can-t-configure-format-on-node-using-media-ctl/m-p/1411447#M186821</link>
    <description>&lt;P&gt;The format you set is not&amp;nbsp; supported.This AN may help you.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13430.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13430.pdf&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Feb 2022 02:11:16 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2022-02-10T02:11:16Z</dc:date>
    <item>
      <title>can't configure format on node using media-ctl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/can-t-configure-format-on-node-using-media-ctl/m-p/1406723#M186463</link>
      <description>&lt;P&gt;i'm trying to set the format for the output of mxc_isi and get an error that I have no idea what it means&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;# media-ctl -V "'mxc_isi.0':12 [fmt:SGRBG8_1X8/1280x720 field:none]"&lt;/SPAN&gt;
&lt;SPAN class=""&gt;Unable to setup formats: No such file or directory (2)&lt;/SPAN&gt;
&lt;/PRE&gt;&lt;P&gt;This is what the nodes look like&lt;/P&gt;&lt;LI-CODE lang="c"&gt;Media controller API version 5.4.70

Media device information
------------------------
driver          mxc-md
model           FSL Capture Media Device
serial          
bus info        
hw revision     0x0
driver version  5.4.70

Device topology
- entity 1: mxc_isi.0 (16 pads, 2 links)
            type V4L2 subdev subtype Unknown flags 0
        pad0: Sink
                &amp;lt;- "mxc-mipi-csi2.0":4 [ENABLED]
        pad1: Sink
        pad2: Sink
        pad3: Sink
        pad4: Sink
        pad5: Sink
        pad6: Sink
        pad7: Sink
        pad8: Sink
        pad9: Sink
        pad10: Sink
        pad11: Sink
        pad12: Source
                -&amp;gt; "mxc_isi.0.capture":0 [ENABLED]
        pad13: Source
        pad14: Source
        pad15: Sink

- entity 18: mxc_isi.0.capture (1 pad, 1 link)
             type Node subtype V4L flags 0
             device node name /dev/video0
        pad0: Sink
                &amp;lt;- "mxc_isi.0":12 [ENABLED]

- entity 22: mxc-mipi-csi2.0 (8 pads, 2 links)
             type Node subtype V4L flags 0
             device node name /dev/v4l-subdev0
        pad0: Sink
                &amp;lt;- "ar0144 2-0010":0 [ENABLED,IMMUTABLE]
        pad1: Sink
        pad2: Sink
        pad3: Sink
        pad4: Source
                -&amp;gt; "mxc_isi.0":0 [ENABLED]
        pad5: Source
        pad6: Source
        pad7: Source

- entity 31: ar0144 2-0010 (2 pads, 1 link)
             type V4L2 subdev subtype Sensor flags 0
             device node name /dev/v4l-subdev1
        pad0: Source
                [fmt:SGRBG12_1X12/1280x720@1/60 field:none colorspace:unknown xfer:none
                 crop.bounds:(0,0)/1296x808
                 crop:(0,4)/1280x720]
                -&amp;gt; "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]
        pad1: Source
                [fmt:SGRBG12_1X12/1280x720@1/60 field:none colorspace:unknown xfer:none
                 crop.bounds:(0,0)/1296x808
                 crop:(0,4)/1280x720]&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jan 2022 17:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/can-t-configure-format-on-node-using-media-ctl/m-p/1406723#M186463</guid>
      <dc:creator>richc128</dc:creator>
      <dc:date>2022-01-28T17:49:15Z</dc:date>
    </item>
    <item>
      <title>Re: can't configure format on node using media-ctl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/can-t-configure-format-on-node-using-media-ctl/m-p/1411447#M186821</link>
      <description>&lt;P&gt;The format you set is not&amp;nbsp; supported.This AN may help you.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13430.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13430.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Feb 2022 02:11:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/can-t-configure-format-on-node-using-media-ctl/m-p/1411447#M186821</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-02-10T02:11:16Z</dc:date>
    </item>
  </channel>
</rss>