<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: mx6 Solo and/or DualLight with two cameras (parallel interface)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mx6-Solo-and-or-DualLight-with-two-cameras-parallel-interface/m-p/235799#M18682</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, this is possible. The second CSI port is mux-ed with EIM signals. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Aug 2013 05:25:03 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2013-08-02T05:25:03Z</dc:date>
    <item>
      <title>mx6 Solo and/or DualLight with two cameras (parallel interface)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx6-Solo-and-or-DualLight-with-two-cameras-parallel-interface/m-p/235798#M18681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible with either the i.mx6 Solo or Dual Light to connect two cameras using two separate parallel interfaces, and receive the two video streams simultaneously? In this application we are not using any display devices, we just want to get the images / video from both cameras into memory. It's not even entirely clear to me whether the Solo has two parallel interfaces, though it seems that the Dual Light definitely does..&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;ilan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2013 16:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx6-Solo-and-or-DualLight-with-two-cameras-parallel-interface/m-p/235798#M18681</guid>
      <dc:creator>ilangoodman</dc:creator>
      <dc:date>2013-08-01T16:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: mx6 Solo and/or DualLight with two cameras (parallel interface)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx6-Solo-and-or-DualLight-with-two-cameras-parallel-interface/m-p/235799#M18682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, this is possible. The second CSI port is mux-ed with EIM signals. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Aug 2013 05:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx6-Solo-and-or-DualLight-with-two-cameras-parallel-interface/m-p/235799#M18682</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-08-02T05:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: mx6 Solo and/or DualLight with two cameras (parallel interface)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx6-Solo-and-or-DualLight-with-two-cameras-parallel-interface/m-p/235800#M18683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yuri. We're making an adapter board to add the second parallel interface to the Boundary Devices SABRE Lite board so we can test this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;** FOLLOW UP **&lt;/P&gt;&lt;P&gt;We've now got two OV5642 (10 bit parallel interface) streaming video simultaneously on the SABRE Lite board with DualLite processor. Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Aug 2013 14:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx6-Solo-and-or-DualLight-with-two-cameras-parallel-interface/m-p/235800#M18683</guid>
      <dc:creator>ilangoodman</dc:creator>
      <dc:date>2013-08-02T14:22:24Z</dc:date>
    </item>
  </channel>
</rss>