<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8MPlus I2S Compatibility</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-I2S-Compatibility/m-p/1410536#M186767</link>
    <description>&lt;P&gt;The IMX8MP have two SYNC signals, for example in SAI3 it have SAI3_RXFS and&amp;nbsp;SAI3_TXFS.&lt;/P&gt;&lt;P&gt;in case we have an audio codec with one bidirectional LRCLK port, to which one of the two signals it should be connected to?&amp;nbsp;SAI3_RXFS or SAI3_TXFS&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Tue, 08 Feb 2022 21:41:24 GMT</pubDate>
    <dc:creator>shifman</dc:creator>
    <dc:date>2022-02-08T21:41:24Z</dc:date>
    <item>
      <title>iMX8MPlus I2S Compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-I2S-Compatibility/m-p/1298219#M176039</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am developing a board with iMX8MPlus processor. I would like to use an audio Codec, TVL320AIC3007, but I have problem with the audio interface between the processor and the Codec.&lt;/P&gt;&lt;P&gt;Here is the interface of the Codec :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GuiDas_0-1624604219575.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147985i608DE803ADDF9DC9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="GuiDas_0-1624604219575.png" alt="GuiDas_0-1624604219575.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;GuiDas_0-1624604219575.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the DIN and DOUT there is no problem as I can use the TX RX data of a SAI. For the clock I am more confused as I need two bidirectionnal clockand the SAI of the processor as only one of them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is, is it possible to connect the Audio Codec to the processor ? If yes which SAI pins can be used for the BCLK and WCLK ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Guilhem&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jun 2021 07:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-I2S-Compatibility/m-p/1298219#M176039</guid>
      <dc:creator>GuiDas</dc:creator>
      <dc:date>2021-06-25T07:07:45Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MPlus I2S Compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-I2S-Compatibility/m-p/1298383#M176046</link>
      <description>&lt;P&gt;Hi Guilhem&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;from TLV320AIC datasheet:&lt;/P&gt;
&lt;P&gt;BCLK - Audio serial data bus bit clock input/output&lt;/P&gt;
&lt;P&gt;WCLK-Audio serial data bus word clock input/output&lt;/P&gt;
&lt;P&gt;BCLK can be connected to SAI BCLK, direction is configured by "BCD" -&lt;/P&gt;
&lt;P&gt;Bit Clock Direction described in sect.14.4&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX8MPRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Plus Applications Processor Reference Manual &lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;WCLK is connected to SAI "Frame Sync" described in sect.14.4.3 External signals&lt;/P&gt;
&lt;P&gt;direction is configured by "FSD"..&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jun 2021 10:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-I2S-Compatibility/m-p/1298383#M176046</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-25T10:06:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MPlus I2S Compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-I2S-Compatibility/m-p/1410536#M186767</link>
      <description>&lt;P&gt;The IMX8MP have two SYNC signals, for example in SAI3 it have SAI3_RXFS and&amp;nbsp;SAI3_TXFS.&lt;/P&gt;&lt;P&gt;in case we have an audio codec with one bidirectional LRCLK port, to which one of the two signals it should be connected to?&amp;nbsp;SAI3_RXFS or SAI3_TXFS&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 08 Feb 2022 21:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-I2S-Compatibility/m-p/1410536#M186767</guid>
      <dc:creator>shifman</dc:creator>
      <dc:date>2022-02-08T21:41:24Z</dc:date>
    </item>
  </channel>
</rss>