<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8M MINI ( pwm1.out pin is  not going low, while shutting down ) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-pwm1-out-pin-is-not-going-low-while-shutting-down/m-p/1409706#M186690</link>
    <description>&lt;P&gt;Dear Nxp Team,&lt;/P&gt;&lt;P&gt;We have realized imx8mini custom board (MIMX8MM4CVTKZAA). we are running android 10 on this board.&lt;/P&gt;&lt;P&gt;We are facing the below issue:&lt;/P&gt;&lt;P&gt;We have interface the processor with display backlight driver(TPS61169DCKR).&lt;/P&gt;&lt;P&gt;&amp;nbsp;To control this backlight we are using pwm1.out(GPIO5_IO05) pin. While shutting down the display we can see 1.54 volts on this pin(pwm1.out[AF8]).&lt;/P&gt;&lt;P&gt;We should get zero volts after shutting down the display, because of this backlight is still on.&lt;/P&gt;&lt;P&gt;When screen is lock/unlock &amp;amp; while controlling brightness pwm1.out pin works totally fine(we are able to see minimum(0v) to maximum(3.3v).&lt;/P&gt;&lt;P&gt;During test we have isolated pwm1.out(AF8) pin from the backlight driver, &amp;amp; found above observations.&lt;/P&gt;&lt;P&gt;Kindly let us know how to control this pwm1.out(AF8) during shutdown.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 07 Feb 2022 13:47:31 GMT</pubDate>
    <dc:creator>siva17290</dc:creator>
    <dc:date>2022-02-07T13:47:31Z</dc:date>
    <item>
      <title>IMX8M MINI ( pwm1.out pin is  not going low, while shutting down )</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-pwm1-out-pin-is-not-going-low-while-shutting-down/m-p/1409706#M186690</link>
      <description>&lt;P&gt;Dear Nxp Team,&lt;/P&gt;&lt;P&gt;We have realized imx8mini custom board (MIMX8MM4CVTKZAA). we are running android 10 on this board.&lt;/P&gt;&lt;P&gt;We are facing the below issue:&lt;/P&gt;&lt;P&gt;We have interface the processor with display backlight driver(TPS61169DCKR).&lt;/P&gt;&lt;P&gt;&amp;nbsp;To control this backlight we are using pwm1.out(GPIO5_IO05) pin. While shutting down the display we can see 1.54 volts on this pin(pwm1.out[AF8]).&lt;/P&gt;&lt;P&gt;We should get zero volts after shutting down the display, because of this backlight is still on.&lt;/P&gt;&lt;P&gt;When screen is lock/unlock &amp;amp; while controlling brightness pwm1.out pin works totally fine(we are able to see minimum(0v) to maximum(3.3v).&lt;/P&gt;&lt;P&gt;During test we have isolated pwm1.out(AF8) pin from the backlight driver, &amp;amp; found above observations.&lt;/P&gt;&lt;P&gt;Kindly let us know how to control this pwm1.out(AF8) during shutdown.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Feb 2022 13:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-pwm1-out-pin-is-not-going-low-while-shutting-down/m-p/1409706#M186690</guid>
      <dc:creator>siva17290</dc:creator>
      <dc:date>2022-02-07T13:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M MINI ( pwm1.out pin is  not going low, while shutting down )</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-pwm1-out-pin-is-not-going-low-while-shutting-down/m-p/1415934#M187189</link>
      <description>&lt;P&gt;The most likely cause of the issue is that, when the display is shutting down, &lt;BR /&gt;the AF8 pad becomes configured as GPIO input, that's why the voltage level on it &lt;BR /&gt;is floating. At that time, it is necessary to configure it as actively driven &lt;BR /&gt;GPIO output and set it to Low state.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Feb 2022 10:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-pwm1-out-pin-is-not-going-low-while-shutting-down/m-p/1415934#M187189</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2022-02-18T10:09:26Z</dc:date>
    </item>
  </channel>
</rss>