<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MXRT1176 OCOTP clock source</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MXRT1176-OCOTP-clock-source/m-p/1406884#M186478</link>
    <description>&lt;P&gt;Thanks a lot for the quick reply and clarification of my question.&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Sun, 30 Jan 2022 15:24:50 GMT</pubDate>
    <dc:creator>alphafred</dc:creator>
    <dc:date>2022-01-30T15:24:50Z</dc:date>
    <item>
      <title>i.MXRT1176 OCOTP clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MXRT1176-OCOTP-clock-source/m-p/1405538#M186351</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to figure out which root clock is supplying the OCOTP peripheral of MIMXRT1176 controller. According to reference manual page 1499 Table 15-5 the clk_enable_ocotp controls LPCG37. However there is no mentioning about LPCG37 in any root clock related chapter/table.&lt;/P&gt;&lt;P&gt;I need this information to calculate the source clock in order to initialize the OCOTP peripheral via OCOTP_Init(OCOTP_Type *base, uint32_t srcClock_Hz).&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 20:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MXRT1176-OCOTP-clock-source/m-p/1405538#M186351</guid>
      <dc:creator>alphafred</dc:creator>
      <dc:date>2022-01-26T20:40:19Z</dc:date>
    </item>
    <item>
      <title>Re: i.MXRT1176 OCOTP clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MXRT1176-OCOTP-clock-source/m-p/1406362#M186418</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;The OCOTP doesn't have the timing control register or similar option to configure.&lt;BR /&gt;So it needn't configure the clock source to drive it and MCU itself is in charge of it.&lt;BR /&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jan 2022 03:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MXRT1176-OCOTP-clock-source/m-p/1406362#M186418</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-01-28T03:16:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.MXRT1176 OCOTP clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MXRT1176-OCOTP-clock-source/m-p/1406884#M186478</link>
      <description>&lt;P&gt;Thanks a lot for the quick reply and clarification of my question.&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Sun, 30 Jan 2022 15:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MXRT1176-OCOTP-clock-source/m-p/1406884#M186478</guid>
      <dc:creator>alphafred</dc:creator>
      <dc:date>2022-01-30T15:24:50Z</dc:date>
    </item>
  </channel>
</rss>