<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multiple Shells? - Virtualisation -  IVSHMEM demo in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1406095#M186405</link>
    <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX28-How-to-set-up-a-SSH-connection-to-EVK-board/m-p/307340" target="_blank"&gt;i.MX28: How to set up a SSH connection to EVK boar... - NXP Community&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Jan 2022 15:01:42 GMT</pubDate>
    <dc:creator>neo2</dc:creator>
    <dc:date>2022-01-27T15:01:42Z</dc:date>
    <item>
      <title>Multiple Shells? - Virtualisation -  IVSHMEM demo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1402820#M186091</link>
      <description>&lt;P&gt;How do I start multiple shells for the&amp;nbsp; IVSHMEM demo?&lt;/P&gt;&lt;P&gt;"uio_read and uio_send need to be started in different shells."&lt;/P&gt;&lt;P&gt;I have Hyperterminal on COM3 where I start U-boot and&amp;nbsp;run jh_mmcboot&lt;/P&gt;&lt;P&gt;"Open two shells, using SSH to log into the board. Execute uio_read in one shell and execute uio_send in the other shell.&lt;BR /&gt;#uio_send /dev/uio0 [count] 0 0&lt;BR /&gt;#uio_read /dev/uio0 [count]"&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 17:52:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1402820#M186091</guid>
      <dc:creator>neo2</dc:creator>
      <dc:date>2022-01-20T17:52:21Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Shells? - Virtualisation -  IVSHMEM demo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1402965#M186109</link>
      <description>&lt;P&gt;You can use ssh connection to open second shell&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 02:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1402965#M186109</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-01-21T02:01:52Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Shells? - Virtualisation -  IVSHMEM demo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1403147#M186129</link>
      <description>&lt;P&gt;Does this mean I use an Ethernet port to ssh into the i.MX8 board rather than the serial port?&lt;BR /&gt;&lt;BR /&gt;Or this can be done using the existing COM4 port?&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 08:54:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1403147#M186129</guid>
      <dc:creator>neo2</dc:creator>
      <dc:date>2022-01-21T08:54:57Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Shells? - Virtualisation -  IVSHMEM demo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1406000#M186397</link>
      <description>&lt;P&gt;I've figured out how to connect a SSH shell using the Ethernet port on the i.MX8 eval board.&lt;/P&gt;&lt;P&gt;In the COM port shell&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;&lt;SPAN&gt;$ ifconfig eth0 up&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;$ ifconfig&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Look for the IP address after inet addr&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;e.g.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;eth0 Link encap:Ethernet HWaddr 00:04:9f:07:15:9a&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;inet addr:169.254.42.78 Bcast:169.254.255.255 Mask:255.255.0.0&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then I start another terminal e.g. I'm using Tera Term to the IP address above&amp;nbsp;&lt;FONT face="courier new,courier"&gt;169.254.42.78&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;The username is root&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jan 2022 11:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1406000#M186397</guid>
      <dc:creator>neo2</dc:creator>
      <dc:date>2022-01-27T11:40:34Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Shells? - Virtualisation -  IVSHMEM demo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1406095#M186405</link>
      <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX28-How-to-set-up-a-SSH-connection-to-EVK-board/m-p/307340" target="_blank"&gt;i.MX28: How to set up a SSH connection to EVK boar... - NXP Community&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jan 2022 15:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1406095#M186405</guid>
      <dc:creator>neo2</dc:creator>
      <dc:date>2022-01-27T15:01:42Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Shells? - Virtualisation -  IVSHMEM demo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1534047#M196102</link>
      <description>&lt;P&gt;Where are the "uio*" executables? They are not in the&amp;nbsp;LF_v5.15.32-2.0.0_images_IMX8MQEVK download, but I got the Linux jailhouse demo working (after some work).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is someone going to update the IMXVIRTUG document?&lt;/P&gt;</description>
      <pubDate>Fri, 07 Oct 2022 18:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-Shells-Virtualisation-IVSHMEM-demo/m-p/1534047#M196102</guid>
      <dc:creator>flobro</dc:creator>
      <dc:date>2022-10-07T18:03:18Z</dc:date>
    </item>
  </channel>
</rss>