<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX7 Solo RTC drift in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1404981#M186318</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196113"&gt;@jindra&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; Generally section 6.1.2.2.1 - Calibrating the time counter - concerns drift in &lt;BR /&gt;the clock, which is used to increment the RTC register. The clock source can be &lt;BR /&gt;any of the following: the internal RC oscillator or RTC_XTAL crystal.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jan 2022 07:39:57 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2022-01-26T07:39:57Z</dc:date>
    <item>
      <title>i.MX7 Solo RTC drift</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1403892#M186189</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I have a question related to the RTC inside the i.MX7 Solo. I'm feeding the RTC_XTALI pin with a 32768 Hz signal generated by another RTC outside of the i.MX7. I'm experiencing drifts between those two RTCs, even though I would expect that they should not drift apart - I though the only cause of a drift would be an oscillator, and that is shared between those two RTCs.&lt;/P&gt;&lt;P&gt;There is a chapter "6.1.2.2.1 - Calibrating the time counter" in the &lt;A href="https://datasheet.datasheetarchive.com/originals/dk/DKDS-17/336112.pdf" target="_self"&gt;reference manual&lt;/A&gt;. I would like to double check if I understand that correctly - this chapter is not about the drift of the internal RC oscillator (which would be used when there would be no signal on the RTC_XTALI pin), but about a drift introduced by the surrounding circuitry of the RTC? I.e. is it the source of the drift we observe with the correct signal on the RTC_XTALI pin?&lt;/P&gt;&lt;P&gt;If so, is this drift temperature dependent?&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jan 2022 10:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1403892#M186189</guid>
      <dc:creator>jindra</dc:creator>
      <dc:date>2022-01-24T10:11:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Solo RTC drift</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1404981#M186318</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196113"&gt;@jindra&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; Generally section 6.1.2.2.1 - Calibrating the time counter - concerns drift in &lt;BR /&gt;the clock, which is used to increment the RTC register. The clock source can be &lt;BR /&gt;any of the following: the internal RC oscillator or RTC_XTAL crystal.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 07:39:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1404981#M186318</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2022-01-26T07:39:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Solo RTC drift</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1405035#M186325</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/1941"&gt;@Yuri&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;thank you for your reply, but it didn't fully explain what I was asking for, so I'll try to rephrase it.&lt;/P&gt;&lt;P&gt;The "clock" you're referring to is generated by a timer, and in my understanding, such timer consists of an oscillator (clock source) and a counter. My question was: &lt;EM&gt;can the counter itself (regardless of the oscillator/clock source used) introduce a drift?&lt;/EM&gt; The chapter 6.1.2.2.1 explicitly says "counter" in the title, but it felt weird to me that the counter itself could introduce a drift - few hardware engineers I talked to said they think it's unlikely.&lt;/P&gt;&lt;P&gt;The other part of my question is "&lt;EM&gt;if the counter itself can introduce a drift, is this drift temperature dependent?&lt;/EM&gt;"&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 09:03:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1405035#M186325</guid>
      <dc:creator>jindra</dc:creator>
      <dc:date>2022-01-26T09:03:00Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Solo RTC drift</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1405069#M186329</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196113"&gt;@jindra&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; main inaccuracy here is provided by crystal oscillator (or RC circuit).&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 09:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1405069#M186329</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2022-01-26T09:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Solo RTC drift</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1406478#M186431</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/1941"&gt;@Yuri&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;you're using the word "&lt;EM&gt;main&lt;/EM&gt;", from which I would conclude that &lt;EM&gt;not all&lt;/EM&gt; the inaccuracy is caused by the oscillator. I am looking for a clear and unambiguous answer to the following question: &lt;EM&gt;can, or can not&lt;/EM&gt;, the counter (i.e. not the oscillator) introduce &lt;EM&gt;some&lt;/EM&gt; amount of drift? If so, is this drift temperature dependent, or will it be constant across a wide range of temperatures?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jindra&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jan 2022 07:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1406478#M186431</guid>
      <dc:creator>jindra</dc:creator>
      <dc:date>2022-01-28T07:44:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Solo RTC drift</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1406511#M186436</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196113"&gt;@jindra&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Power supply ripple can affect digital part of circuits.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jan 2022 09:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Solo-RTC-drift/m-p/1406511#M186436</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2022-01-28T09:04:55Z</dc:date>
    </item>
  </channel>
</rss>