<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT1021: Writing to flash when running XIP from the same flash. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1021-Writing-to-flash-when-running-XIP-from-the-same-flash/m-p/1404644#M186270</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there a way to write/program the&amp;nbsp;&lt;EM&gt;same&lt;/EM&gt; flash that you are running XIP from?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Ronnie&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jan 2022 15:15:48 GMT</pubDate>
    <dc:creator>rshipman</dc:creator>
    <dc:date>2022-01-25T15:15:48Z</dc:date>
    <item>
      <title>RT1021: Writing to flash when running XIP from the same flash.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1021-Writing-to-flash-when-running-XIP-from-the-same-flash/m-p/1404644#M186270</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there a way to write/program the&amp;nbsp;&lt;EM&gt;same&lt;/EM&gt; flash that you are running XIP from?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Ronnie&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 15:15:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1021-Writing-to-flash-when-running-XIP-from-the-same-flash/m-p/1404644#M186270</guid>
      <dc:creator>rshipman</dc:creator>
      <dc:date>2022-01-25T15:15:48Z</dc:date>
    </item>
    <item>
      <title>Re: RT1021: Writing to flash when running XIP from the same flash.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1021-Writing-to-flash-when-running-XIP-from-the-same-flash/m-p/1404876#M186297</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is there a way to write/program the same flash that you are running XIP from?&lt;BR /&gt;-- Yes, it's possible on the condition that relocating the FlexSPI driver in the RAM and you can refer to the flexspi_nor_polling_transfer demo in the SDK library to do it.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 02:34:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1021-Writing-to-flash-when-running-XIP-from-the-same-flash/m-p/1404876#M186297</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-01-26T02:34:53Z</dc:date>
    </item>
    <item>
      <title>Re: RT1021: Writing to flash when running XIP from the same flash.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1021-Writing-to-flash-when-running-XIP-from-the-same-flash/m-p/1696986#M210070</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56840"&gt;@jeremyzhou&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I am very interested on this topic.&lt;/P&gt;&lt;P&gt;When you say:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;on the condition that relocating the FlexSPI driver in the RAM&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;How that can be achieved with details? I have taken a look to the example you mention: &lt;EM&gt;flexspi_nor_polling_transfer&amp;nbsp;&lt;/EM&gt;and I see&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;FlexSPI driver is moved to RAM on the Linker (linkscripts folder)&lt;/LI&gt;&lt;LI&gt;Use another Flash driver that the most common one:&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Selrac_13_0-1690927186114.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/234608i3ECF503D24C88E97/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Selrac_13_0-1690927186114.png" alt="Selrac_13_0-1690927186114.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Selrac_13_0-1690927186114.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But I don't see any Flash partitions or anything like that.&lt;/P&gt;&lt;P&gt;My current project is using this other flash driver:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Selrac_13_1-1690927265895.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/234609i883FB4D471E41F68/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Selrac_13_1-1690927265895.png" alt="Selrac_13_1-1690927265895.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Selrac_13_1-1690927265895.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Having the&amp;nbsp;&lt;EM&gt;MIMXRT1020-EVK_IS25LP064.cfx&lt;/EM&gt; is a requirement?&lt;/P&gt;&lt;P&gt;With more details what I want to achieve is to use the 8 MB SPI Flash for different purposes:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;3 MB for the program itself&lt;/LI&gt;&lt;LI&gt;Other 5 MB as a Flash storage to use in RAW to read/write data&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Which steps I need to follow?&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Carles&lt;/P&gt;</description>
      <pubDate>Tue, 01 Aug 2023 22:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1021-Writing-to-flash-when-running-XIP-from-the-same-flash/m-p/1696986#M210070</guid>
      <dc:creator>Selrac_13</dc:creator>
      <dc:date>2023-08-01T22:28:31Z</dc:date>
    </item>
  </channel>
</rss>