<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6ULL-evk use Murata CYW43455 module with BUILDROOT in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evk-use-Murata-CYW43455-module-with-BUILDROOT/m-p/1404529#M186256</link>
    <description>&lt;P&gt;Hi everybody,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to setup Murata Wifi Module&amp;nbsp;CYW43455-1MW (I have the uSD-M2 Adapter kit) on my iMX6ULL-14x14-evk dev board, and I'm using &lt;STRONG&gt;Buildroot&lt;/STRONG&gt;&amp;nbsp;(version 2021-08-01) as build system. I easily found murata-cyw-fw inside the packages and set my dts for dev board imx6ull-14x14-evk-btwifi.dts . but I can't still see anything in the OS running. Except for the usdhc messages:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[ 38.053537] mmc0: queuing unknown CIS tuple 0x80 (2 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.068525] mmc0: queuing unknown CIS tuple 0x80 (3 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.081181] mmc0: queuing unknown CIS tuple 0x80 (3 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.099778] mmc0: queuing unknown CIS tuple 0x80 (7 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.116583] mmc0: queuing unknown CIS tuple 0x80 (6 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.393765] mmc0: new ultra high speed SDR104 SDIO card at address 0001&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Does anybody have exceprience with this module and how to it up with buildroot?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks so much&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Simone&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jan 2022 11:03:17 GMT</pubDate>
    <dc:creator>SicScar</dc:creator>
    <dc:date>2022-01-25T11:03:17Z</dc:date>
    <item>
      <title>iMX6ULL-evk use Murata CYW43455 module with BUILDROOT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evk-use-Murata-CYW43455-module-with-BUILDROOT/m-p/1404529#M186256</link>
      <description>&lt;P&gt;Hi everybody,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to setup Murata Wifi Module&amp;nbsp;CYW43455-1MW (I have the uSD-M2 Adapter kit) on my iMX6ULL-14x14-evk dev board, and I'm using &lt;STRONG&gt;Buildroot&lt;/STRONG&gt;&amp;nbsp;(version 2021-08-01) as build system. I easily found murata-cyw-fw inside the packages and set my dts for dev board imx6ull-14x14-evk-btwifi.dts . but I can't still see anything in the OS running. Except for the usdhc messages:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[ 38.053537] mmc0: queuing unknown CIS tuple 0x80 (2 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.068525] mmc0: queuing unknown CIS tuple 0x80 (3 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.081181] mmc0: queuing unknown CIS tuple 0x80 (3 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.099778] mmc0: queuing unknown CIS tuple 0x80 (7 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.116583] mmc0: queuing unknown CIS tuple 0x80 (6 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 38.393765] mmc0: new ultra high speed SDR104 SDIO card at address 0001&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Does anybody have exceprience with this module and how to it up with buildroot?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks so much&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Simone&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 11:03:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evk-use-Murata-CYW43455-module-with-BUILDROOT/m-p/1404529#M186256</guid>
      <dc:creator>SicScar</dc:creator>
      <dc:date>2022-01-25T11:03:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ULL-evk use Murata CYW43455 module with BUILDROOT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evk-use-Murata-CYW43455-module-with-BUILDROOT/m-p/1408740#M186611</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191770"&gt;@SicScar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unfortunate buildroot is not officially supported by NXP, you could ask on the community from Murata and see of they do, or wait for feedback that has experience on this tool.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Feb 2022 19:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evk-use-Murata-CYW43455-module-with-BUILDROOT/m-p/1408740#M186611</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2022-02-03T19:15:20Z</dc:date>
    </item>
  </channel>
</rss>