<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SPI communication on MCIMX8M-EVKB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-communication-on-MCIMX8M-EVKB/m-p/1404499#M186250</link>
    <description>&lt;P&gt;Replying to my own question.&lt;BR /&gt;&lt;BR /&gt;Based on what I seen on the schematic I don't see a suitable point SPI interfaces&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;1. the ECSPI interfaces are being used up by the board itself for it's own chips&lt;/P&gt;&lt;P&gt;2. the QSPI interface is just for Flash rather than a generic SPI. I don't see MOSI and MISO on that interface.&lt;BR /&gt;&lt;BR /&gt;I'll probably used the Ethernet interface instead.&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jan 2022 10:07:24 GMT</pubDate>
    <dc:creator>neo2</dc:creator>
    <dc:date>2022-01-25T10:07:24Z</dc:date>
    <item>
      <title>SPI communication on MCIMX8M-EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-communication-on-MCIMX8M-EVKB/m-p/1403933#M186195</link>
      <description>&lt;P&gt;Dear NXP&lt;/P&gt;&lt;P&gt;I have an MCIMX8M-EVKB board.&lt;/P&gt;&lt;P&gt;Is there a location where SPI is available to connect to another NXP board?&lt;BR /&gt;&lt;BR /&gt;The only header I see is J801 but that only seems to have a I2C interface.&lt;/P&gt;&lt;P&gt;Or is it is not possible to connect the&amp;nbsp;MCIMX8M board as there are no spare SPI headers or points to connect the 4 wires?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Lee.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jan 2022 11:26:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-communication-on-MCIMX8M-EVKB/m-p/1403933#M186195</guid>
      <dc:creator>neo2</dc:creator>
      <dc:date>2022-01-24T11:26:26Z</dc:date>
    </item>
    <item>
      <title>Re: SPI communication on MCIMX8M-EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-communication-on-MCIMX8M-EVKB/m-p/1404499#M186250</link>
      <description>&lt;P&gt;Replying to my own question.&lt;BR /&gt;&lt;BR /&gt;Based on what I seen on the schematic I don't see a suitable point SPI interfaces&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;1. the ECSPI interfaces are being used up by the board itself for it's own chips&lt;/P&gt;&lt;P&gt;2. the QSPI interface is just for Flash rather than a generic SPI. I don't see MOSI and MISO on that interface.&lt;BR /&gt;&lt;BR /&gt;I'll probably used the Ethernet interface instead.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 10:07:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-communication-on-MCIMX8M-EVKB/m-p/1404499#M186250</guid>
      <dc:creator>neo2</dc:creator>
      <dc:date>2022-01-25T10:07:24Z</dc:date>
    </item>
    <item>
      <title>Re: SPI communication on MCIMX8M-EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-communication-on-MCIMX8M-EVKB/m-p/1411279#M186815</link>
      <description>&lt;P&gt;Hi Neo,&lt;/P&gt;
&lt;P&gt;No, this board does not have an SPI port. yes you could the ethernet.&lt;/P&gt;
&lt;P&gt;Best Regards.&lt;/P&gt;
&lt;P&gt;Diego.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 18:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-communication-on-MCIMX8M-EVKB/m-p/1411279#M186815</guid>
      <dc:creator>Juan-Rodarte</dc:creator>
      <dc:date>2022-02-09T18:39:47Z</dc:date>
    </item>
  </channel>
</rss>