<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: ECSPI transfer gets stuck after 3 bytes</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1403207#M186135</link>
    <description>&lt;P&gt;Which SDK are you using? Which board are you using?&lt;/P&gt;
&lt;P&gt;Have you try other examples in the SDK and still have the issue?&lt;/P&gt;</description>
    <pubDate>Fri, 21 Jan 2022 10:30:06 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2022-01-21T10:30:06Z</dc:date>
    <item>
      <title>ECSPI transfer gets stuck after 3 bytes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1400186#M185899</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;We are using the ECSPI2 in the i.mx8 m mini from the M4 core.&lt;/P&gt;&lt;P&gt;ECSPI2 is disabled in the device tree so that the M4 has full control.&lt;/P&gt;&lt;P&gt;The SPI is configured to transfer 5 bytes with the&amp;nbsp;ECSPI_MasterTransferNonBlocking and then generate the&amp;nbsp;RXFIFO Data Request Interrupt.&lt;/P&gt;&lt;P&gt;This works fine for some time but at some point the SPI Transfer hangs after sending 3 byte.&lt;/P&gt;&lt;P&gt;What could cause ECSPI to only transfer 3 byte?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers Marcel&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 09:36:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1400186#M185899</guid>
      <dc:creator>MBaer</dc:creator>
      <dc:date>2022-01-17T09:36:32Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI transfer gets stuck after 3 bytes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1403207#M186135</link>
      <description>&lt;P&gt;Which SDK are you using? Which board are you using?&lt;/P&gt;
&lt;P&gt;Have you try other examples in the SDK and still have the issue?&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 10:30:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1403207#M186135</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-01-21T10:30:06Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI transfer gets stuck after 3 bytes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1404423#M186240</link>
      <description>&lt;P&gt;Hi Jimmy&lt;/P&gt;&lt;P&gt;We are using SDK 2.11.0 with a custom board using the i.MX8M Mini.&lt;/P&gt;&lt;P&gt;I could fix the original issue by using the CMSIS implementation of the ECSPI.&lt;/P&gt;&lt;P&gt;But there i face an other issue, that i cannot use ecspi2 and ecspi3 simultaneously.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used the cmsis_ecspi_int_loopback_transfer as starting point and implemented ecspi 3 accordingly. I can use the ecspi3 alone but not both together.&lt;/P&gt;&lt;P&gt;Either the ECSPI2_DriverIRQHandler or the&amp;nbsp;ECSPI3_DriverIRQHandler is not triggered.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 08:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1404423#M186240</guid>
      <dc:creator>MBaer</dc:creator>
      <dc:date>2022-01-25T08:19:54Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI transfer gets stuck after 3 bytes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1405201#M186337</link>
      <description>&lt;P&gt;I added the NvicInit() and now it works on both spis.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 13:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-transfer-gets-stuck-after-3-bytes/m-p/1405201#M186337</guid>
      <dc:creator>MBaer</dc:creator>
      <dc:date>2022-01-26T13:37:53Z</dc:date>
    </item>
  </channel>
</rss>