<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Boot is delayed 30 seconds on cold boot imx8</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1401238#M185979</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195763"&gt;@Amelius&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Does this issue exist on customer board?&lt;/P&gt;</description>
    <pubDate>Wed, 19 Jan 2022 02:23:05 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2022-01-19T02:23:05Z</dc:date>
    <item>
      <title>Boot is delayed 30 seconds on cold boot imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1401012#M185965</link>
      <description>&lt;P&gt;Hey,&lt;/P&gt;&lt;P&gt;I'm experiencing a strange behavior during a cold start up (the device is disconnected from power longer than 2 Minutes and than powered up). The boot up is delayed right after "ddrc freq set to low bus mode" by 30s twice (see log) and the total boot time is around 80s.&lt;/P&gt;&lt;P&gt;If the device is rebooted or just unplugged and plugged for less than 20 seconds, the boot time is around 15s&lt;/P&gt;&lt;P&gt;Processor: i.MX 8M&lt;/P&gt;&lt;P&gt;Greetings&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 15:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1401012#M185965</guid>
      <dc:creator>Amelius</dc:creator>
      <dc:date>2022-01-18T15:08:40Z</dc:date>
    </item>
    <item>
      <title>Re: Boot is delayed 30 seconds on cold boot imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1401238#M185979</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195763"&gt;@Amelius&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Does this issue exist on customer board?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jan 2022 02:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1401238#M185979</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-01-19T02:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: Boot is delayed 30 seconds on cold boot imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1401568#M185996</link>
      <description>&lt;P&gt;Yes, it's a customer board&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 08:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1401568#M185996</guid>
      <dc:creator>Amelius</dc:creator>
      <dc:date>2022-01-20T08:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: Boot is delayed 30 seconds on cold boot imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1402154#M186032</link>
      <description>&lt;P&gt;Try to redo ddr test.This issue relates to ddr hardware design.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 02:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1402154#M186032</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-01-20T02:07:26Z</dc:date>
    </item>
    <item>
      <title>Re: Boot is delayed 30 seconds on cold boot imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1417683#M187355</link>
      <description>&lt;P&gt;After further investigation I came to the conclusion that the behavior occurs after adding the RT kernel patch patch-5.4.3-rt1 and the kernel config options&amp;nbsp;CONFIG_EMBEDDED=y and CONFIG_PREEMPT_RT=y&lt;/P&gt;&lt;P&gt;adding&amp;nbsp;&lt;BR /&gt;CONFIG_CPU_FREQ_DEFAULT_GOV_PERFORMANCE=y&lt;BR /&gt;CONFIG_DEVFREQ_GOV_PERFORMANCE=y&lt;BR /&gt;didn't bring an improvement&lt;/P&gt;&lt;P&gt;it doesn't look like it has to do with the ddr hardware design since the manufacture did extensiv tests with the mentioned tool&lt;/P&gt;&lt;P&gt;&lt;A href="https://cdn.kernel.org/pub/linux/kernel/projects/rt/5.4/older/" target="_blank"&gt;Index of /pub/linux/kernel/projects/rt/5.4/older/&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 18:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-is-delayed-30-seconds-on-cold-boot-imx8/m-p/1417683#M187355</guid>
      <dc:creator>Amelius</dc:creator>
      <dc:date>2022-02-22T18:51:17Z</dc:date>
    </item>
  </channel>
</rss>