<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX 8M Plus Support for USB on Cortex-M7 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Support-for-USB-on-Cortex-M7/m-p/1401114#M185974</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, there is no driver available for USB&amp;nbsp;available in the official SDK release.&lt;BR /&gt;&lt;BR /&gt;It may be possible to port it from other devices for example i.MXRT, but the PHY and USB non-core registers are different, and it will not be straightforward to port.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Tue, 18 Jan 2022 19:41:48 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-01-18T19:41:48Z</dc:date>
    <item>
      <title>i.MX 8M Plus Support for USB on Cortex-M7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Support-for-USB-on-Cortex-M7/m-p/1399633#M185841</link>
      <description>&lt;P&gt;I'm looking for support for interfacing with a USB device from the Cortex-M7 coprocessor of the IMX8Plus.&lt;BR /&gt;&lt;BR /&gt;I am using this SMARC board here from Avnet:&amp;nbsp;&lt;A href="https://www.msc-technologies.eu/support/boards/smarc/msc-sm2s-imx8plus.html" target="_blank"&gt;https://www.msc-technologies.eu/support/boards/smarc/msc-sm2s-imx8plus.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Along with this carrier board from Congatec:&amp;nbsp;&lt;A href="https://www.congatec.com/us/products/accessories/conga-seval/" target="_blank"&gt;https://www.congatec.com/us/products/accessories/conga-seval/&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;From the system running on the A53 processor (Linux) I have access to both USB ports. We would like access to one of the ports from the M7.&lt;BR /&gt;&lt;BR /&gt;Using the SDK SDK_2_10_0_MIMX8ML8xxxKZ I cannot find any USB drivers or examples for this use case. Does this require pin remapping? Does the Cortex-M7 even support IO? Are there other SDKs that contain drivers and middleware that are needed?&lt;BR /&gt;&lt;BR /&gt;Any information or solutions to this along with more information on utilizing the Cortex-M7 would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 21:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Support-for-USB-on-Cortex-M7/m-p/1399633#M185841</guid>
      <dc:creator>cwembedded1</dc:creator>
      <dc:date>2022-01-14T21:00:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus Support for USB on Cortex-M7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Support-for-USB-on-Cortex-M7/m-p/1401114#M185974</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, there is no driver available for USB&amp;nbsp;available in the official SDK release.&lt;BR /&gt;&lt;BR /&gt;It may be possible to port it from other devices for example i.MXRT, but the PHY and USB non-core registers are different, and it will not be straightforward to port.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 19:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Support-for-USB-on-Cortex-M7/m-p/1401114#M185974</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-01-18T19:41:48Z</dc:date>
    </item>
  </channel>
</rss>