<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックEthernet eDMA Driver for IMIXRT1170</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-eDMA-Driver-for-IMIXRT1170/m-p/1400726#M185941</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;We want to use eDMA for ethernet in our project in IMIXRT1170. Is there any driver for ethernet eDMA for this Processor. If no, then how to use eDMA for ethernet.&lt;/P&gt;&lt;P&gt;We saw eDMA driver for various peripherals like LPUART, FlexIO etc. but this is not available for ethernet. Is there any specific reason behind that.&lt;/P&gt;&lt;P&gt;Tools Used:&lt;/P&gt;&lt;P&gt;IDE: MCUxpresso v11.4.1&lt;/P&gt;&lt;P&gt;SDK 2.10.1&lt;/P&gt;</description>
    <pubDate>Tue, 18 Jan 2022 07:11:41 GMT</pubDate>
    <dc:creator>nishantraaz</dc:creator>
    <dc:date>2022-01-18T07:11:41Z</dc:date>
    <item>
      <title>Ethernet eDMA Driver for IMIXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-eDMA-Driver-for-IMIXRT1170/m-p/1400726#M185941</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;We want to use eDMA for ethernet in our project in IMIXRT1170. Is there any driver for ethernet eDMA for this Processor. If no, then how to use eDMA for ethernet.&lt;/P&gt;&lt;P&gt;We saw eDMA driver for various peripherals like LPUART, FlexIO etc. but this is not available for ethernet. Is there any specific reason behind that.&lt;/P&gt;&lt;P&gt;Tools Used:&lt;/P&gt;&lt;P&gt;IDE: MCUxpresso v11.4.1&lt;/P&gt;&lt;P&gt;SDK 2.10.1&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 07:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-eDMA-Driver-for-IMIXRT1170/m-p/1400726#M185941</guid>
      <dc:creator>nishantraaz</dc:creator>
      <dc:date>2022-01-18T07:11:41Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet eDMA Driver for IMIXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-eDMA-Driver-for-IMIXRT1170/m-p/1400804#M185955</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195867"&gt;@nishantraaz&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; i.MX RT1170 ENET has own unified DMA (uDMA), internal to the ENET module, which&lt;BR /&gt;optimizes data transfer between the ENET core and the SoC, and supports an enhanced &lt;BR /&gt;buffer descriptor programming model to support IEEE 1588 functionality.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; There is no need for eDMA.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 09:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-eDMA-Driver-for-IMIXRT1170/m-p/1400804#M185955</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2022-01-18T09:09:22Z</dc:date>
    </item>
  </channel>
</rss>