<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: umx6ul SOM bootloader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1399662#M185843</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You may refer to the i.MX6UL EVK schematic and compare with your custom hardware.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=MCIMX6UL-EVK_DESIGNFILES" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=MCIMX6UL-EVK_DESIGNFILES&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Also, you could try using UUU available for download here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.4.165" target="_blank"&gt;https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.4.165&lt;/A&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Using this tool you may download uboot as well, you'll need to enable fastboot utilities in uboot for the tool to be able to flash.&lt;BR /&gt;&lt;BR /&gt;Also, you could use the tool to check if the device has been detected by running the command:&lt;BR /&gt;./uuu.exe -lsusb&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jan 2022 22:25:15 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-01-14T22:25:15Z</dc:date>
    <item>
      <title>umx6ul SOM bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1398880#M185761</link>
      <description>&lt;P&gt;Hi. I try to load bootloader to custom board with imx6ul SOM. Usb dont find by host, so imx-usb-loader dont load anything to device. What am i doing wrong, what i should look into?&lt;BR /&gt;Use 69, 70 pin for USB_N, USB_P, 76 for USB_OTG2_ID. Boot mode 0 on 103 pin, 1 on 104 pin (serial downloader).&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 13:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1398880#M185761</guid>
      <dc:creator>JustTryToDoJob</dc:creator>
      <dc:date>2022-01-13T13:19:02Z</dc:date>
    </item>
    <item>
      <title>Re: umx6ul SOM bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1399073#M185783</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please note that imx-usb-loader is not supported by NXP, if you find further issues with this please consider asking in their github.&lt;BR /&gt;&lt;BR /&gt;Does the host PC not detect the USB connected in serial download?&lt;BR /&gt;Or is it that the imx-usb-loader does not find the device?&lt;BR /&gt;&lt;BR /&gt;If it is the second. Please try the mentioned here:&lt;BR /&gt;&lt;A href="https://github.com/boundarydevices/imx_usb_loader/issues/105" target="_blank"&gt;https://github.com/boundarydevices/imx_usb_loader/issues/105&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 20:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1399073#M185783</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-01-13T20:23:55Z</dc:date>
    </item>
    <item>
      <title>Re: umx6ul SOM bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1399085#M185785</link>
      <description>&lt;P&gt;It is the first - host dont detect usb. I use this -&amp;nbsp;&lt;A href="https://www.phytec.eu/documents/l-844e-1-phyboard-segin-bsp-manual/#Booting_from_USB_OTG_.28Serial_Downloader.29" target="_self"&gt;phytec&lt;/A&gt;&amp;nbsp;as a manual to flash my software. What are other problematic moments may it be? USB ID pin? What are other soft i can use to flash the bootloader?&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 21:08:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1399085#M185785</guid>
      <dc:creator>JustTryToDoJob</dc:creator>
      <dc:date>2022-01-13T21:08:03Z</dc:date>
    </item>
    <item>
      <title>Re: umx6ul SOM bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1399662#M185843</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You may refer to the i.MX6UL EVK schematic and compare with your custom hardware.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=MCIMX6UL-EVK_DESIGNFILES" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=MCIMX6UL-EVK_DESIGNFILES&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Also, you could try using UUU available for download here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.4.165" target="_blank"&gt;https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.4.165&lt;/A&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Using this tool you may download uboot as well, you'll need to enable fastboot utilities in uboot for the tool to be able to flash.&lt;BR /&gt;&lt;BR /&gt;Also, you could use the tool to check if the device has been detected by running the command:&lt;BR /&gt;./uuu.exe -lsusb&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 22:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/umx6ul-SOM-bootloader/m-p/1399662#M185843</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-01-14T22:25:15Z</dc:date>
    </item>
  </channel>
</rss>