<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using UART3_TXD (GPIO5[27]) as an GPIO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399645#M185842</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using i.MX 8M Mini Processor.&lt;/P&gt;&lt;P&gt;I cannot use UART3_TXD (GPIO5[27]) as an GPIO.&lt;/P&gt;&lt;P&gt;What could be the problem?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Adde&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jan 2022 21:35:21 GMT</pubDate>
    <dc:creator>adde_ado</dc:creator>
    <dc:date>2022-01-14T21:35:21Z</dc:date>
    <item>
      <title>Using UART3_TXD (GPIO5[27]) as an GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399645#M185842</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using i.MX 8M Mini Processor.&lt;/P&gt;&lt;P&gt;I cannot use UART3_TXD (GPIO5[27]) as an GPIO.&lt;/P&gt;&lt;P&gt;What could be the problem?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Adde&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 21:35:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399645#M185842</guid>
      <dc:creator>adde_ado</dc:creator>
      <dc:date>2022-01-14T21:35:21Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART3_TXD (GPIO5[27]) as an GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399670#M185844</link>
      <description>&lt;P&gt;Hi Adde&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;reason may be that it is used by other driver/application. One can try to set manually&lt;/P&gt;
&lt;P&gt;using jtag debugger or memtool&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=lf-5.10.72_2.2.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=lf-5.10.72_2.2.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Another reason may be that chip is broken, probably due to ESD or overheating.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 23:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399670#M185844</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2022-01-14T23:35:38Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART3_TXD (GPIO5[27]) as an GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399712#M185854</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for your previous answer.&lt;/P&gt;&lt;P&gt;What about this post?&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO3-24-as-an-GPIO/m-p/375613" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO3-24-as-an-GPIO/m-p/375613&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Could it be the same problem I am experiencing?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Adde&lt;/P&gt;</description>
      <pubDate>Sat, 15 Jan 2022 07:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399712#M185854</guid>
      <dc:creator>adde_ado</dc:creator>
      <dc:date>2022-01-15T07:40:51Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART3_TXD (GPIO5[27]) as an GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399716#M185856</link>
      <description>&lt;P&gt;&amp;gt;What about this post?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;that post talks about UART3_TXD which is connected to external part&lt;/P&gt;
&lt;P&gt;and that part(configured as output) drives UART3_TXD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sat, 15 Jan 2022 08:17:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399716#M185856</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2022-01-15T08:17:09Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART3_TXD (GPIO5[27]) as an GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399726#M185860</link>
      <description>&lt;P&gt;see&lt;/P&gt;</description>
      <pubDate>Sat, 15 Jan 2022 13:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO5-27-as-an-GPIO/m-p/1399726#M185860</guid>
      <dc:creator>josephzhou1</dc:creator>
      <dc:date>2022-01-15T13:59:53Z</dc:date>
    </item>
  </channel>
</rss>