<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: some problem with imx233 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/some-problem-with-imx233/m-p/235411#M18582</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cheng youping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI, the mp3 encoding issue is resolved in community and you can apply the solution at &lt;A href="https://community.nxp.com/message/382609"&gt;Can't encode mp3 on imx28&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Mar 2014 06:19:23 GMT</pubDate>
    <dc:creator>PeterChan</dc:creator>
    <dc:date>2014-03-17T06:19:23Z</dc:date>
    <item>
      <title>some problem with imx233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/some-problem-with-imx233/m-p/235409#M18580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;download updated imx233 bsp and install ltib,&lt;/P&gt;&lt;P&gt;1. ltib gst-plugin have no mfw_mp3_encoder.&lt;/P&gt;&lt;P&gt;setup was as following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;./ltib -c&lt;/P&gt;&lt;P&gt;select gst-plugin,gstream -plug-base,gst-plug-good, CFimager the imx23_linux.sb and rootfs.ext.gz 's content to sd card,boot imx233 dvk,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@freescale"&gt;root@freescale&lt;/A&gt; ~$ cd /&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@freescale"&gt;root@freescale&lt;/A&gt; /$ gst-inspect |grep mfw&lt;/P&gt;&lt;P&gt;mfw_mpeg4aspdecoder:&amp;nbsp; mfw_mpeg4aspdecoder: Freescale MPEG4 Decoder&lt;/P&gt;&lt;P&gt;mfw_v4lsink:&amp;nbsp; mfw_v4lsink: Freescale: V4L Sink&lt;/P&gt;&lt;P&gt;mfw_aacdecoder:&amp;nbsp; mfw_aacdecoder: Freescale AAC Decoder Plugin&lt;/P&gt;&lt;P&gt;mfw_mp3decoder:&amp;nbsp; mfw_mp3decoder: freescale mp3 decoder&lt;/P&gt;&lt;P&gt;mfw_mp4demuxer:&amp;nbsp; mfw_mp4demuxer: FSL MP4 Demuxer&lt;/P&gt;&lt;P&gt;mfw_avidemuxer:&amp;nbsp; mfw_avidemuxer: FSL Avi Demuxer&lt;/P&gt;&lt;P&gt;mfw_h264decoder:&amp;nbsp; mfw_h264decoder: Freescale&amp;nbsp;&amp;nbsp;&amp;nbsp; H264 decoder&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@freescale"&gt;root@freescale&lt;/A&gt; /$&lt;/P&gt;&lt;P&gt;//no mfw_mp3encoder: freescale mp3 encoder,can't excute mp3 encoder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. select&lt;/P&gt;&lt;P&gt;./ltib -c&lt;/P&gt;&lt;P&gt;select fsl-mm-codec-libs and fsl-mm-mp3enc-libs&lt;/P&gt;&lt;P&gt;can't get fsl-mm-mp3enc-codeclib.1.8.0.tar.gz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;./ltib -c&lt;/P&gt;&lt;P&gt;select fsl-mm-codec-libs only.&lt;/P&gt;&lt;P&gt;no test_mp3_enc_arm9_elinux and lib_mp3_enc_arm9_elinux.so&lt;/P&gt;&lt;P&gt;can't exectue mp3 encode either..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;download updated imx28 multimedai framework.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;L2.6.35_1.1.0_130130_MM_CODECS_BUNDLE.tar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;re-install ltib.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the result is as attachment.&lt;/P&gt;&lt;P&gt;all in one word,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are some error in imx233/imx28 mp3 encoder,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could someone help me ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 10:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/some-problem-with-imx233/m-p/235409#M18580</guid>
      <dc:creator>chengyouping</dc:creator>
      <dc:date>2014-02-14T10:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: some problem with imx233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/some-problem-with-imx233/m-p/235410#M18581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The codec package fsl-mm-1.80.tar.gz does not possess the mfw_mp3encoder element and thus mp3 encode is not supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried the L2.6.35_1.1.0_130130_MM_CODECS on BSP L2.6.35_1.1.0 using i.MX28 and got similar errors. It looks mp3 encode do not work in i.MX233 &amp;amp; i.MX28.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 10:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/some-problem-with-imx233/m-p/235410#M18581</guid>
      <dc:creator>PeterChan</dc:creator>
      <dc:date>2014-02-25T10:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: some problem with imx233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/some-problem-with-imx233/m-p/235411#M18582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cheng youping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI, the mp3 encoding issue is resolved in community and you can apply the solution at &lt;A href="https://community.nxp.com/message/382609"&gt;Can't encode mp3 on imx28&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Mar 2014 06:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/some-problem-with-imx233/m-p/235411#M18582</guid>
      <dc:creator>PeterChan</dc:creator>
      <dc:date>2014-03-17T06:19:23Z</dc:date>
    </item>
  </channel>
</rss>