<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX8MP with 16-bit LPDDR4 setting problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-with-16-bit-LPDDR4-setting-problem/m-p/1398683#M185744</link>
    <description>&lt;P&gt;OK, thank you for your reply.&lt;/P&gt;</description>
    <pubDate>Thu, 13 Jan 2022 07:22:10 GMT</pubDate>
    <dc:creator>simonng</dc:creator>
    <dc:date>2022-01-13T07:22:10Z</dc:date>
    <item>
      <title>iMX8MP with 16-bit LPDDR4 setting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-with-16-bit-LPDDR4-setting-problem/m-p/1395944#M185507</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;I tried to set the single channel setting and run it on the 8MP EVKB (8MPLUSLPD4-EVK). Then I used the DDR Tool to run the Stress Test. But the test hang up. I noticed that the Col size is changed to 11 and the density per chip select is still 3072MB. I attached the ds file and RPA file. Can you help me to check this problem? I can apply the single channel setting on the iMX8MQ but not the iMX8MP.&lt;/P&gt;&lt;P&gt;Here is the log:&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;ARM clock(CA53) rate: 1800MHz&lt;BR /&gt;DDR Clock: 2000MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;DDR type is LPDDR4&lt;BR /&gt;Data width: 16, bank num: 8&lt;BR /&gt;Row size: 17, col size: 11&lt;/P&gt;&lt;P&gt;Note: though not necessarily in error, it is normally unusual&lt;BR /&gt;to have a number of column address bits exceed 10. It is recommended&lt;BR /&gt;to double check the DRAM data sheet to ensure the correct column count and&lt;BR /&gt;to set unused column address bits in registers ADDRMAP3 and ADDRMAP4 to 0xF&lt;BR /&gt;or else the there will be a miscalculation of the total density&lt;/P&gt;&lt;P&gt;Two chip selects are used&lt;BR /&gt;Number of DDR controllers used on the SoC: 1&lt;BR /&gt;Density per chip select: 3072MB&lt;BR /&gt;Density per controller is: 6144MB&lt;BR /&gt;Total density detected on the board is: 6144MB&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;MX8M-plus: Cortex-A53 is found&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;============ Step 1: DDRPHY Training... ============&lt;BR /&gt;---DDR 1D-Training @2000Mhz...&lt;BR /&gt;[Process] End of CA training&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;[Process] End of read DQ deskew training&lt;BR /&gt;[Process] End of MPR read delay center optimization&lt;BR /&gt;[Process] End of Write Leveling coarse delay&lt;BR /&gt;[Process] End of write delay center optimization&lt;BR /&gt;[Process] End of read delay center optimization&lt;BR /&gt;[Process] End of max read latency training&lt;BR /&gt;[Result] PASS&lt;BR /&gt;---DDR 1D-Training @200Mhz...&lt;BR /&gt;[Process] End of CA training&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;[Process] End of MPR read delay center optimization&lt;BR /&gt;[Process] End of Write Leveling coarse delay&lt;BR /&gt;[Process] End of write delay center optimization&lt;BR /&gt;[Process] End of read delay center optimization&lt;BR /&gt;[Process] End of max read latency training&lt;BR /&gt;[Result] PASS&lt;BR /&gt;---DDR 1D-Training @50Mhz...&lt;BR /&gt;[Process] End of CA training&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;[Process] End of MPR read delay center optimization&lt;BR /&gt;[Process] End of Write Leveling coarse delay&lt;BR /&gt;[Process] End of write delay center optimization&lt;BR /&gt;[Process] End of read delay center optimization&lt;BR /&gt;[Process] End of max read latency training&lt;BR /&gt;[Result] PASS&lt;BR /&gt;---DDR 2D-Training @2000Mhz...&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of 2D write delay/voltage center optimization&lt;BR /&gt;[Process] End of 2D read delay/voltage center optimization&lt;BR /&gt;[Result] PASS&lt;/P&gt;&lt;P&gt;============ Step 2: DDR memory accessing... ============&lt;BR /&gt;Verifying DDR frequency point0@2000MHz.......Pass&lt;BR /&gt;Verifying DDR frequency point1@200MHz.......Pass&lt;BR /&gt;Verifying DDR frequency point2@50MHz.......Pass&lt;BR /&gt;[Result] OK&lt;/P&gt;&lt;P&gt;============ Step 3: DDR parameters processing... ============&lt;BR /&gt;[Result] Done&lt;/P&gt;&lt;P&gt;Success: DDR Calibration completed!!!&lt;BR /&gt;DDR Stress Test Iteration 1&lt;BR /&gt;--------------------------------&lt;BR /&gt;--Running DDR test on region 1--&lt;BR /&gt;--------------------------------&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 06:21:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-with-16-bit-LPDDR4-setting-problem/m-p/1395944#M185507</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2022-01-07T06:21:40Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP with 16-bit LPDDR4 setting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-with-16-bit-LPDDR4-setting-problem/m-p/1396487#M185559</link>
      <description>&lt;P&gt;The i.MX8MP is different from i.MX8MQ, the i.MX8MQ support 16/32-bit DRAM Interface, but for the i.MX8MP support 32-bit DRAM Interface.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 03:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-with-16-bit-LPDDR4-setting-problem/m-p/1396487#M185559</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2022-01-10T03:00:00Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP with 16-bit LPDDR4 setting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-with-16-bit-LPDDR4-setting-problem/m-p/1398683#M185744</link>
      <description>&lt;P&gt;OK, thank you for your reply.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 07:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-with-16-bit-LPDDR4-setting-problem/m-p/1398683#M185744</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2022-01-13T07:22:10Z</dc:date>
    </item>
  </channel>
</rss>