<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAdding External interrupt to RT1170 platform.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Adding-External-interrupt-to-RT1170-platform/m-p/1398218#M185713</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to interrupt RT1170 (running MCUxpresso) from another board using a gpio line. With the limited exposed pins on RT1170 connectors (all pins of J9,J10, J25, J26), which pins in connectors J9,J10, J25, J26 can be used for this purpose. I am looking at something similar to &lt;EM&gt;evkmimxrt1170_igpio_input_interrupt_cm7&lt;/EM&gt; project where the interrupt is connected to a dedicated WAKEUP pin, that is something i don't want to use.&lt;/P&gt;&lt;P&gt;Going through the pin config tools seem never ending complex process to me. Any help is highly appreciable. Thanks in advance.&lt;/P&gt;&lt;P&gt;-Krishna&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jan 2022 16:18:41 GMT</pubDate>
    <dc:creator>krishnad</dc:creator>
    <dc:date>2022-01-12T16:18:41Z</dc:date>
    <item>
      <title>Adding External interrupt to RT1170 platform.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-External-interrupt-to-RT1170-platform/m-p/1398218#M185713</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to interrupt RT1170 (running MCUxpresso) from another board using a gpio line. With the limited exposed pins on RT1170 connectors (all pins of J9,J10, J25, J26), which pins in connectors J9,J10, J25, J26 can be used for this purpose. I am looking at something similar to &lt;EM&gt;evkmimxrt1170_igpio_input_interrupt_cm7&lt;/EM&gt; project where the interrupt is connected to a dedicated WAKEUP pin, that is something i don't want to use.&lt;/P&gt;&lt;P&gt;Going through the pin config tools seem never ending complex process to me. Any help is highly appreciable. Thanks in advance.&lt;/P&gt;&lt;P&gt;-Krishna&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 16:18:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-External-interrupt-to-RT1170-platform/m-p/1398218#M185713</guid>
      <dc:creator>krishnad</dc:creator>
      <dc:date>2022-01-12T16:18:41Z</dc:date>
    </item>
    <item>
      <title>Re: Adding External interrupt to RT1170 platform.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-External-interrupt-to-RT1170-platform/m-p/1402131#M186030</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well. &lt;BR /&gt;I suggest you use Config Tools to configure the pins in GPIO, at the Label column you can see which connector the board has assigned for a specific pin. E.g. here GPIO11_IO11 is routed to J9[4]:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_0-1642639046183.png" style="width: 472px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168254i9EBD7769A1CFA5B5/image-dimensions/472x271?v=v2" width="472" height="271" role="button" title="Omar_Anguiano_0-1642639046183.png" alt="Omar_Anguiano_0-1642639046183.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Omar_Anguiano_0-1642639046183.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;To configure the specific interrupts you can do it based on the example provided in the SDK modifying the macro's value to match your used GPIO´s.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 00:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-External-interrupt-to-RT1170-platform/m-p/1402131#M186030</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-01-20T00:38:19Z</dc:date>
    </item>
  </channel>
</rss>