<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8qxp : After change debug uart, can't work kernel. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-After-change-debug-uart-can-t-work-kernel/m-p/1397849#M185688</link>
    <description>&lt;P&gt;When I check source code,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think it has error abou "stdout-path" in&amp;nbsp;&lt;SPAN&gt;early_init_dt_scan_chosen_stdout(), driver/of/fdt.c&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jan 2022 06:06:05 GMT</pubDate>
    <dc:creator>brian_kim</dc:creator>
    <dc:date>2022-01-12T06:06:05Z</dc:date>
    <item>
      <title>imx8qxp : After change debug uart, can't work kernel.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-After-change-debug-uart-can-t-work-kernel/m-p/1397676#M185679</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I changed debug port from uart0 to uart1,&lt;/P&gt;&lt;P&gt;u-boot is normal. ( I can see debug messages.)&lt;/P&gt;&lt;P&gt;After load kernel and dtb, I can't check debug message.&lt;/P&gt;&lt;P&gt;=&amp;gt; setenv mmcargs 'setenv bootargs console=ttyLP1,115200 earlycon=lpuart32,0x5a070000,115200 root=${mmcroot}'&lt;BR /&gt;=&amp;gt; boot&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0(part 0) is current device&lt;BR /&gt;Failed to load 'boot.scr'&lt;BR /&gt;28770816 bytes read in 108 ms (254.1 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;92860 bytes read in 2 ms (44.3 MiB/s)&lt;BR /&gt;Moving Image from 0x80280000 to 0x80400000, end=82000000&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 0000000083000000, end 0000000083019abb&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think kernel into unlimited loop.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;power supply&lt;/P&gt;&lt;P&gt;Normal boot : about 450mA&lt;/P&gt;&lt;P&gt;Now : (Start kernel) -&amp;gt; over 400mA -&amp;gt; 200~300ms -&amp;gt; 370mA (holding)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can't see kernel message and&amp;nbsp;I can't access ssh with eth0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I solve this issue ?&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 01:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-After-change-debug-uart-can-t-work-kernel/m-p/1397676#M185679</guid>
      <dc:creator>brian_kim</dc:creator>
      <dc:date>2022-01-12T01:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp : After change debug uart, can't work kernel.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-After-change-debug-uart-can-t-work-kernel/m-p/1397849#M185688</link>
      <description>&lt;P&gt;When I check source code,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think it has error abou "stdout-path" in&amp;nbsp;&lt;SPAN&gt;early_init_dt_scan_chosen_stdout(), driver/of/fdt.c&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 06:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-After-change-debug-uart-can-t-work-kernel/m-p/1397849#M185688</guid>
      <dc:creator>brian_kim</dc:creator>
      <dc:date>2022-01-12T06:06:05Z</dc:date>
    </item>
  </channel>
</rss>