<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx258 serial upload protocol</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx258-serial-upload-protocol/m-p/1397431#M185657</link>
    <description>&lt;P&gt;Hello mkffm2k22,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You should receive address in ROM and not in DDR, please check it:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4547.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4547.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jan 2022 14:04:35 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2022-01-11T14:04:35Z</dc:date>
    <item>
      <title>imx258 serial upload protocol</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx258-serial-upload-protocol/m-p/1394192#M185352</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I am investigating some imx258 boards where I don't understand the current state of the imx258 chip.&lt;/P&gt;&lt;P&gt;The boards should be virgin, so I am using the serial upload protocol to talk to the imx258.&lt;BR /&gt;Write Memory with len 4, address 0xB8001004 and value 0x0076E83f returns ack 0x12343412, followed by 0x128a8a12.&lt;/P&gt;&lt;P&gt;My understanding is that this is the correct response if the board has secure boot enabled (if not, I should see 0x56787856 and 0x128a8a12). I tried a couple of Read Memory commands, all of them failed, regardless of the address. Again, this is the expected behaviour for imx258 chips with secure boot enabled.&lt;/P&gt;&lt;P&gt;The problem is, however, that the boards are meant to be at factory defaults and secure boot should&lt;BR /&gt;be disabled. Do you have any idea what I could do to get more information about the imx258's state?&lt;/P&gt;&lt;P&gt;I tried uploading a firmware image that is signed and known to work on our boards. The upload works ok, the final Completed command returns 0x88888888 as expected. But the firmware does not start.&lt;BR /&gt;I then sent a Get Status after the Completed command, this returned four times 0x47 (SRK hash does not match the uploaded image).&lt;/P&gt;&lt;P&gt;Is it ok in general to send a Get Status command after a firmware upload and the final Completed command? In an error case as above, I get a status of the failed upload, But if the upload and the firmware verification worked ok, the firmware is now beeing run and the imx258 does not respond&lt;BR /&gt;to Get Status (or other serial upload protocol commands) any more. Is it ok to use a timeout of a final Get Status as indication that the firmware upload was successful?&lt;/P&gt;&lt;P&gt;Thanks in advance for your comments.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jan 2022 10:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx258-serial-upload-protocol/m-p/1394192#M185352</guid>
      <dc:creator>mkffm2k22</dc:creator>
      <dc:date>2022-01-04T10:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx258 serial upload protocol</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx258-serial-upload-protocol/m-p/1397431#M185657</link>
      <description>&lt;P&gt;Hello mkffm2k22,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You should receive address in ROM and not in DDR, please check it:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4547.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4547.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 14:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx258-serial-upload-protocol/m-p/1397431#M185657</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-01-11T14:04:35Z</dc:date>
    </item>
  </channel>
</rss>