<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8 Instrument Cluster Android 11 not displaying in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Instrument-Cluster-Android-11-not-displaying/m-p/1396948#M185616</link>
    <description>&lt;P&gt;I am having an issue where the instrument cluster does not come up on the secondary display. The screen will either simply not stay on after displaying the loading animation or it will mirror the other display.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the iMX8QM board running Android Automotive version 11.0.0_2.3.0 from NXP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the mek_8q_car-userdebug lunch command.&lt;/P&gt;&lt;P&gt;The instrument cluster display is plugged into the LVDS1_CH0 and has a display ratio of 1920x720.&lt;/P&gt;&lt;P&gt;The main display is plugged into the LVDS0_CH0 port and has a resolution of 1920x1080.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I plug in a different display with a 1920x1080 resolution the instrument cluster works properly but I need to use the 1920x720 display.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a config file or something I have to change for this? It works when I swap the two displays and it worked fine with Android 10.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jan 2022 01:58:10 GMT</pubDate>
    <dc:creator>SL239</dc:creator>
    <dc:date>2022-01-11T01:58:10Z</dc:date>
    <item>
      <title>i.MX8 Instrument Cluster Android 11 not displaying</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Instrument-Cluster-Android-11-not-displaying/m-p/1396948#M185616</link>
      <description>&lt;P&gt;I am having an issue where the instrument cluster does not come up on the secondary display. The screen will either simply not stay on after displaying the loading animation or it will mirror the other display.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the iMX8QM board running Android Automotive version 11.0.0_2.3.0 from NXP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the mek_8q_car-userdebug lunch command.&lt;/P&gt;&lt;P&gt;The instrument cluster display is plugged into the LVDS1_CH0 and has a display ratio of 1920x720.&lt;/P&gt;&lt;P&gt;The main display is plugged into the LVDS0_CH0 port and has a resolution of 1920x1080.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I plug in a different display with a 1920x1080 resolution the instrument cluster works properly but I need to use the 1920x720 display.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a config file or something I have to change for this? It works when I swap the two displays and it worked fine with Android 10.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 01:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Instrument-Cluster-Android-11-not-displaying/m-p/1396948#M185616</guid>
      <dc:creator>SL239</dc:creator>
      <dc:date>2022-01-11T01:58:10Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Instrument Cluster Android 11 not displaying</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Instrument-Cluster-Android-11-not-displaying/m-p/1397054#M185635</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194793"&gt;@SL239&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you attach the kernel drm log(need to open drm debug mode) and android log?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 05:17:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Instrument-Cluster-Android-11-not-displaying/m-p/1397054#M185635</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-01-11T05:17:58Z</dc:date>
    </item>
  </channel>
</rss>