<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RE: Remote Debug QT5 User Guide in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1395455#M185471</link>
    <description>&lt;P&gt;Are you mix up the package install to your target image and the package you needed to build the image on your Ubuntu Host?&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jan 2022 07:59:59 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2022-01-06T07:59:59Z</dc:date>
    <item>
      <title>RE: Remote Debug QT5 User Guide</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1393602#M185270</link>
      <description>&lt;P&gt;I read the User Guide ,&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Remote-debug-QT5-User-Guide/ta-p/1391161" target="_blank" rel="noopener"&gt;Remote debug QT5 User Guide - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1 Change local.conf file in Yocto&lt;BR /&gt;CORE_IMAGE_EXTRA_INSTALL += "openssh openssh-sftp openssh-sftp-server"&lt;BR /&gt;EXTRA_IMAGE_FEATURES = "dev-pkgs debug-tweaks tools-debug ssh-server-openssh "&lt;BR /&gt;IMAGE_INSTALL_append += "net-tools iputils dhcpcd which gzip python python-pip wget cmake \&lt;BR /&gt;git gtk+ zlib patchelf nano grep tmux swig tar unzip parted e2fsprogs e2fsprogs-resize2fs \&lt;BR /&gt;openssh rsync"&lt;BR /&gt;2 Build and deploy Yocto SDK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BUT&amp;nbsp;&amp;nbsp;&lt;FONT color="#FF0000"&gt;which&amp;nbsp;grep tar&amp;nbsp; etc.&lt;/FONT&gt; all r build in Ubuntu rite&amp;gt; and&amp;nbsp;&lt;/P&gt;&lt;P&gt;i tok wget&amp;nbsp; and curl and unzip&amp;nbsp; python3 etc. all are installed during the process to build yocto bsp , see renference . not need re install again ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;see "Linux Current Relese" here ,&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_blank" rel="noopener"&gt;i.MX Yocto Project User’s Guide​&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;3.2 Host packages&lt;BR /&gt;A Yocto Project build requires that some packages be installed for the build that are documented under the Yocto Project. Go to&lt;BR /&gt;Yocto Project Quick Start and check for the packages that must be installed for your build machine.&lt;BR /&gt;Essential Yocto Project host packages are:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;$ sudo apt-get install gawk &lt;FONT color="#FF0000"&gt;wget&lt;/FONT&gt; git-core diffstat &lt;FONT face="arial black,avant garde" color="#FF0000"&gt;&lt;STRONG&gt;unzip&lt;/STRONG&gt;&lt;/FONT&gt; texinfo gcc-multilib \&lt;BR /&gt;build-essential chrpath socat cpio python &lt;FONT color="#FF0000"&gt;python3&lt;/FONT&gt; python3-pip python3-pexpect \&lt;BR /&gt;xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \&lt;BR /&gt;pylint3 xterm &lt;FONT color="#FF0000"&gt;rsync curl&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The configuration tool uses the default version of grep that is on your build machine. If there is a different version of grep in your&lt;BR /&gt;path, it may cause builds to fail. One workaround is to rename the special version to something not containing "grep".&lt;BR /&gt;3.3 Setting up the Repo utility&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please advice me ???&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 13:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1393602#M185270</guid>
      <dc:creator>josephzhou1</dc:creator>
      <dc:date>2022-01-06T13:55:54Z</dc:date>
    </item>
    <item>
      <title>Re: RE: Remote Debug QT5 User Guide</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1395455#M185471</link>
      <description>&lt;P&gt;Are you mix up the package install to your target image and the package you needed to build the image on your Ubuntu Host?&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 07:59:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1395455#M185471</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-01-06T07:59:59Z</dc:date>
    </item>
    <item>
      <title>Re: RE: Remote Debug QT5 User Guide</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1395635#M185483</link>
      <description>&lt;P&gt;No. i never.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2&lt;/P&gt;&lt;P&gt;here i am only talking about the tools (or the Host Packages ) only , never ever even touch the " target image " topic.&lt;/P&gt;&lt;P&gt;if talk about target image it is also the same : many packages are already have you no need "append" them:)&lt;/P&gt;&lt;P&gt;if u append this may be ok&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;IMAGE_INSTALL_append += “ opencv opencv-samples”&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;for necessary functions&lt;/P&gt;&lt;P&gt;3&lt;/P&gt;&lt;P&gt;i found out they do "double installation" (hence a waste ) some of the host packages , and the guy&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788" target="_self"&gt;&lt;SPAN class=""&gt;nxf65025&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;have already&amp;nbsp; replied&amp;nbsp; me with a confirmed&amp;nbsp; Private Message . his answer which make me happy , he said&amp;nbsp; "Yes"&amp;nbsp; to my suggestion.&amp;nbsp;&lt;/P&gt;&lt;P&gt;4&lt;/P&gt;&lt;P&gt;i have done many GDB debugging myself, either in command line or in IDE Eclipse in past few months, so I understand that for the target image itself , actually only need "gdbserver" only for run and (ip:192.168.1.253)connected back to the host ubuntu machine(ip: 192.168.1.252) , all GDB function and also symbols all are located in the host . hence save memory for the target . so better not installed so many packages into target totally&amp;nbsp; &amp;nbsp;,&amp;nbsp; thanks all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;gdbserver 192.168.1.252:2001&amp;nbsp; XYZ ( here the binary file is XYZ)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;$GDB XYZs( here the same binary with symbols)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;5&lt;/P&gt;&lt;P&gt;thank you , we keep in touch , make progress together, thank you thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 06:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1395635#M185483</guid>
      <dc:creator>josephzhou1</dc:creator>
      <dc:date>2022-01-12T06:04:38Z</dc:date>
    </item>
    <item>
      <title>Re: RE: Remote Debug QT5 User Guide</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1395996#M185515</link>
      <description>&lt;P&gt;Yes, keep in touch. If you need any further help, please let us know.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 07:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RE-Remote-Debug-QT5-User-Guide/m-p/1395996#M185515</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-01-07T07:18:47Z</dc:date>
    </item>
  </channel>
</rss>