<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6 and libcamera in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-and-libcamera/m-p/1394874#M185445</link>
    <description>&lt;P&gt;Hello bschuste,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Depend of the camera, if it usb then it should work, however the bsp comes with OV4640.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jan 2022 14:55:26 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2022-01-05T14:55:26Z</dc:date>
    <item>
      <title>i.MX6 and libcamera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-and-libcamera/m-p/1394403#M185381</link>
      <description>&lt;P&gt;I am trying to use libcamera on a Boundary Devices (BD-SL-i.MX6) holding kernel 5.15.2 from&amp;nbsp;github.com/Freescale/linux-fslc commit&amp;nbsp;3b7c3ba50480.&lt;/P&gt;&lt;P&gt;Is there a recommended libcamera version known to work with this kernel?&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jan 2022 20:24:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-and-libcamera/m-p/1394403#M185381</guid>
      <dc:creator>bschuste</dc:creator>
      <dc:date>2022-01-04T20:24:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 and libcamera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-and-libcamera/m-p/1394874#M185445</link>
      <description>&lt;P&gt;Hello bschuste,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Depend of the camera, if it usb then it should work, however the bsp comes with OV4640.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 14:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-and-libcamera/m-p/1394874#M185445</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-01-05T14:55:26Z</dc:date>
    </item>
  </channel>
</rss>