<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 32bit libg2d in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/32bit-libg2d/m-p/1394258#M185361</link>
    <description>&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;Our application (which is 32-bit) wants to use functions from libg2d which in our iMX8QXP CPU is provided by the recipe imx-dpu-g2d (In Yocto). The provided binary library is however a 64-bit version which we cannot link against. We have tried installing a 32-bit version by prepending the recipe name with lib32 (as is normally done to make Yocto build the corresponding 32-bit version of a recipe), but then Yocto tries to download a file prepended with lib32 (lib32-imx-dpu-g2d-1.7.6.bin) which is not available. Is there any other way to get a 32-bit version of the libg2d library for an iMX8QXP CPU?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Jonners.&lt;/P&gt;</description>
    <pubDate>Tue, 04 Jan 2022 13:06:35 GMT</pubDate>
    <dc:creator>jonners_guttman</dc:creator>
    <dc:date>2022-01-04T13:06:35Z</dc:date>
    <item>
      <title>32bit libg2d</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/32bit-libg2d/m-p/1394258#M185361</link>
      <description>&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;Our application (which is 32-bit) wants to use functions from libg2d which in our iMX8QXP CPU is provided by the recipe imx-dpu-g2d (In Yocto). The provided binary library is however a 64-bit version which we cannot link against. We have tried installing a 32-bit version by prepending the recipe name with lib32 (as is normally done to make Yocto build the corresponding 32-bit version of a recipe), but then Yocto tries to download a file prepended with lib32 (lib32-imx-dpu-g2d-1.7.6.bin) which is not available. Is there any other way to get a 32-bit version of the libg2d library for an iMX8QXP CPU?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Jonners.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jan 2022 13:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/32bit-libg2d/m-p/1394258#M185361</guid>
      <dc:creator>jonners_guttman</dc:creator>
      <dc:date>2022-01-04T13:06:35Z</dc:date>
    </item>
    <item>
      <title>Re: 32bit libg2d</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/32bit-libg2d/m-p/1394876#M185446</link>
      <description>&lt;P&gt;Hello jonners,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry the iMX8x is a 64 bit architecture, all you find will be in 64 bits. There is a version of 32 bit of the library but is for MX6Q.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 14:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/32bit-libg2d/m-p/1394876#M185446</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-01-05T14:57:51Z</dc:date>
    </item>
  </channel>
</rss>