<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6Q-CustomBoard- PMIC Issue while sdcard flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-CustomBoard-PMIC-Issue-while-sdcard-flash/m-p/1393830#M185304</link>
    <description>&lt;P&gt;Hi NXP&amp;nbsp; ,&lt;BR /&gt;&lt;BR /&gt;Custom board is reference of sabresd quad processor .&lt;BR /&gt;&lt;BR /&gt;Changes from sabresd board to custom board is PMIC,DDR,UART,USDHC etc . We have handled all the changes but still Facing PMIC issue .i.e&amp;nbsp;&lt;BR /&gt;"&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;U-Boot 2018.03-dirty (Jan 03 2022 - 15:41:04 +0530)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;CPU: Freescale i.MX6Q rev1.3 at 792MHz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;CPU: Industrial temperature grade (-40C to 105C) at 21C&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;Reset cause: POR&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;Model: Freescale i.MX6 Quad SABRE Smart Device Board&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;Board: MX6-CustomBoardName&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;DRAM: 2 GiB&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;i2c_idle_bus: failed to clear bus, sda=1 scl=0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;PMIC: PFUZE100! DEV_ID=0xffffffda REV_ID=0xffffffda&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;initcall sequence 8ffa539c failed at call 17804afc (err=-19)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;### ERROR ### Please RESET the board ###&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The following voltages are different from the reference Sabre SDB board and are set in the file /uboot-imx/board/freescale/mx6qcustomboard/mx6qcustomboard.c:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;• SW2 is set to 3.3V • SW4 is set to 1.975V • VGEN5 is set to 2.8V • VGEN6 is set to 3.3V&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* Set SW4 to 1.975V - Address of SW4VOLT is 0x4A */&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg =&amp;nbsp;pmic_reg_read(dev,0x4A);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg &amp;amp;= ~0x3F;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg |= 0x3F;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pmic_reg_write(dev,0x4A,reg);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* SW4 setup done */&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg =&amp;nbsp;pmic_reg_read(dev, 0x35);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg &amp;amp;= ~0x3F;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg |= 0x32;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pmic_reg_write(dev,0x35,reg);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg =&amp;nbsp;pmic_reg_read(dev, 0x70);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg &amp;amp;= ~0xf;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg |= 0xa;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pmic_reg_write(dev,0x70, reg);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/*increase VGEN3 from 2.5 to 2.8V*/&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg =&amp;nbsp;pmic_reg_read(dev, 0x6e);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg &amp;amp;= ~0xF;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg |= 0xA;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pmic_reg_write(dev, 0x6e,reg);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* VGEN3 setup done */&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Let me know other than&amp;nbsp;&lt;SPAN&gt;mx6qcustomboard.c Is there any other place I need to handle?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jan 2022 16:57:37 GMT</pubDate>
    <dc:creator>laulavanya</dc:creator>
    <dc:date>2022-01-03T16:57:37Z</dc:date>
    <item>
      <title>IMX6Q-CustomBoard- PMIC Issue while sdcard flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-CustomBoard-PMIC-Issue-while-sdcard-flash/m-p/1393830#M185304</link>
      <description>&lt;P&gt;Hi NXP&amp;nbsp; ,&lt;BR /&gt;&lt;BR /&gt;Custom board is reference of sabresd quad processor .&lt;BR /&gt;&lt;BR /&gt;Changes from sabresd board to custom board is PMIC,DDR,UART,USDHC etc . We have handled all the changes but still Facing PMIC issue .i.e&amp;nbsp;&lt;BR /&gt;"&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;U-Boot 2018.03-dirty (Jan 03 2022 - 15:41:04 +0530)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;CPU: Freescale i.MX6Q rev1.3 at 792MHz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;CPU: Industrial temperature grade (-40C to 105C) at 21C&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;Reset cause: POR&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;Model: Freescale i.MX6 Quad SABRE Smart Device Board&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;Board: MX6-CustomBoardName&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;DRAM: 2 GiB&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;i2c_idle_bus: failed to clear bus, sda=1 scl=0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;PMIC: PFUZE100! DEV_ID=0xffffffda REV_ID=0xffffffda&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;initcall sequence 8ffa539c failed at call 17804afc (err=-19)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde" size="2" color="#993300"&gt;### ERROR ### Please RESET the board ###&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The following voltages are different from the reference Sabre SDB board and are set in the file /uboot-imx/board/freescale/mx6qcustomboard/mx6qcustomboard.c:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;• SW2 is set to 3.3V • SW4 is set to 1.975V • VGEN5 is set to 2.8V • VGEN6 is set to 3.3V&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* Set SW4 to 1.975V - Address of SW4VOLT is 0x4A */&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg =&amp;nbsp;pmic_reg_read(dev,0x4A);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg &amp;amp;= ~0x3F;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg |= 0x3F;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pmic_reg_write(dev,0x4A,reg);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* SW4 setup done */&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg =&amp;nbsp;pmic_reg_read(dev, 0x35);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg &amp;amp;= ~0x3F;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg |= 0x32;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pmic_reg_write(dev,0x35,reg);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg =&amp;nbsp;pmic_reg_read(dev, 0x70);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg &amp;amp;= ~0xf;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg |= 0xa;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pmic_reg_write(dev,0x70, reg);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/*increase VGEN3 from 2.5 to 2.8V*/&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg =&amp;nbsp;pmic_reg_read(dev, 0x6e);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg &amp;amp;= ~0xF;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;reg |= 0xA;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pmic_reg_write(dev, 0x6e,reg);&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* VGEN3 setup done */&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Let me know other than&amp;nbsp;&lt;SPAN&gt;mx6qcustomboard.c Is there any other place I need to handle?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jan 2022 16:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-CustomBoard-PMIC-Issue-while-sdcard-flash/m-p/1393830#M185304</guid>
      <dc:creator>laulavanya</dc:creator>
      <dc:date>2022-01-03T16:57:37Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q-CustomBoard- PMIC Issue while sdcard flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-CustomBoard-PMIC-Issue-while-sdcard-flash/m-p/1393879#M185314</link>
      <description>&lt;P&gt;Hi Lavanya&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Let me know other than mx6qcustomboard.c Is there any other place I need to handle?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;from log issue may be related to i2c interface, so one can check it with oscilloscope.&lt;/P&gt;
&lt;P&gt;Also may be recommended to check pmic connections using Chapter&amp;nbsp;4&lt;BR /&gt;Requirements for Power Management&amp;nbsp; &lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jan 2022 23:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-CustomBoard-PMIC-Issue-while-sdcard-flash/m-p/1393879#M185314</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2022-01-03T23:16:36Z</dc:date>
    </item>
  </channel>
</rss>