<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX7 PCI-E root error on Linux 5.10</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-PCI-E-root-error-on-Linux-5-10/m-p/1393564#M185260</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I have trouble with PCI-E root on IMX7Dual. Sometimes (appr. 10-20% of runnings) PCI-E root initialization failed. In dmesg is printed:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;[ 5.743604] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.753563] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;BR /&gt;[ 5.760722] pcieport 0000:01:00.0: enabling device (0140 -&amp;gt; 0143)&lt;BR /&gt;[ 5.767816] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.777715] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;BR /&gt;[ 5.784297] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.794141] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;BR /&gt;[ 5.800725] pcieport 0000:02:01.0: enabling device (0140 -&amp;gt; 0143)&lt;BR /&gt;[ 5.815680] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.826639] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;BR /&gt;[ 5.833205] pcieport 0000:02:02.0: enabling device (0140 -&amp;gt; 0143)&lt;BR /&gt;[ 5.846646] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.857934] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Meanwhile on the bus there are two ethernet adapter and their driver hangs. If initialization of PCI-E root is successful then ethernet works perfectly.&lt;/P&gt;&lt;P&gt;lspci printing if error occures:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;00:00.0 Non-VGA unclassified device: Synopsys, Inc. DWC_usb3 / PCIe bridge (rev 01)&lt;BR /&gt;01:00.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:01.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:02.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:03.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;03:00.0 Ethernet controller: Intel Corporation I210 Gigabit Unprogrammed (rev 03)&lt;BR /&gt;04:00.0 Ethernet controller: Intel Corporation I210 Gigabit Unprogrammed (rev 03)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;lspci printing if all right:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;00:00.0 PCI bridge: Synopsys, Inc. DWC_usb3 / PCIe bridge (rev 01)&lt;BR /&gt;01:00.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:01.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:02.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:03.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;03:00.0 Ethernet controller: Intel Corporation I210 Gigabit Unprogrammed (rev 03)&lt;BR /&gt;04:00.0 Ethernet controller: Intel Corporation I210 Gigabit Unprogrammed (rev 03)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Linux kernel version 5.10.88 from here:&lt;/P&gt;&lt;P&gt;git clone -b git.kernel.org/linux-stable/linux-5.10.y &lt;A href="https://source.codeaurora.org/external/imx/linux-imx" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If I use version of kernel 4.14 then error doesn't appear.&lt;/P&gt;&lt;P&gt;What problem is this?&lt;/P&gt;&lt;P&gt;In attachment: config of kernel, dmesg | grep -i 'pci' if error occures (log_bad.txt) and doesn't (log_good.txt).&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 31 Dec 2021 17:04:28 GMT</pubDate>
    <dc:creator>mst31</dc:creator>
    <dc:date>2021-12-31T17:04:28Z</dc:date>
    <item>
      <title>IMX7 PCI-E root error on Linux 5.10</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-PCI-E-root-error-on-Linux-5-10/m-p/1393564#M185260</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I have trouble with PCI-E root on IMX7Dual. Sometimes (appr. 10-20% of runnings) PCI-E root initialization failed. In dmesg is printed:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;[ 5.743604] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.753563] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;BR /&gt;[ 5.760722] pcieport 0000:01:00.0: enabling device (0140 -&amp;gt; 0143)&lt;BR /&gt;[ 5.767816] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.777715] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;BR /&gt;[ 5.784297] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.794141] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;BR /&gt;[ 5.800725] pcieport 0000:02:01.0: enabling device (0140 -&amp;gt; 0143)&lt;BR /&gt;[ 5.815680] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.826639] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;BR /&gt;[ 5.833205] pcieport 0000:02:02.0: enabling device (0140 -&amp;gt; 0143)&lt;BR /&gt;[ 5.846646] pci 0000:00:00.0: can't enable device: BAR 0 [mem 0x00000000-0x000fffff 64bit pref] not claimed&lt;BR /&gt;[ 5.857934] pci 0000:00:00.0: Error enabling bridge (-22), continuing&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Meanwhile on the bus there are two ethernet adapter and their driver hangs. If initialization of PCI-E root is successful then ethernet works perfectly.&lt;/P&gt;&lt;P&gt;lspci printing if error occures:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;00:00.0 Non-VGA unclassified device: Synopsys, Inc. DWC_usb3 / PCIe bridge (rev 01)&lt;BR /&gt;01:00.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:01.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:02.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:03.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;03:00.0 Ethernet controller: Intel Corporation I210 Gigabit Unprogrammed (rev 03)&lt;BR /&gt;04:00.0 Ethernet controller: Intel Corporation I210 Gigabit Unprogrammed (rev 03)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;lspci printing if all right:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;00:00.0 PCI bridge: Synopsys, Inc. DWC_usb3 / PCIe bridge (rev 01)&lt;BR /&gt;01:00.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:01.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:02.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;02:03.0 PCI bridge: Pericom Semiconductor PI7C9X2G404 EL/SL PCIe2 4-Port/4-Lane Packet Switch (rev 05)&lt;BR /&gt;03:00.0 Ethernet controller: Intel Corporation I210 Gigabit Unprogrammed (rev 03)&lt;BR /&gt;04:00.0 Ethernet controller: Intel Corporation I210 Gigabit Unprogrammed (rev 03)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Linux kernel version 5.10.88 from here:&lt;/P&gt;&lt;P&gt;git clone -b git.kernel.org/linux-stable/linux-5.10.y &lt;A href="https://source.codeaurora.org/external/imx/linux-imx" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If I use version of kernel 4.14 then error doesn't appear.&lt;/P&gt;&lt;P&gt;What problem is this?&lt;/P&gt;&lt;P&gt;In attachment: config of kernel, dmesg | grep -i 'pci' if error occures (log_bad.txt) and doesn't (log_good.txt).&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 31 Dec 2021 17:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-PCI-E-root-error-on-Linux-5-10/m-p/1393564#M185260</guid>
      <dc:creator>mst31</dc:creator>
      <dc:date>2021-12-31T17:04:28Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7 PCI-E root error on Linux 5.10</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-PCI-E-root-error-on-Linux-5-10/m-p/1393640#M185278</link>
      <description>&lt;P&gt;Hi Mikhail&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;how many boards affected by that issue, if this is one board this may be soldering issue.&lt;/P&gt;
&lt;P&gt;Also may be recommended to check hardware using attached Hardware Development Guide.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sun, 02 Jan 2022 23:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-PCI-E-root-error-on-Linux-5-10/m-p/1393640#M185278</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2022-01-02T23:43:53Z</dc:date>
    </item>
  </channel>
</rss>