<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: support for docker on i.MX8MP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/support-for-docker-on-i-MX8MP/m-p/1391128#M184919</link>
    <description>&lt;P&gt;You can see this test docker image and it's readme:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://hub.docker.com/repository/docker/fdsgfn/ubuntu21.04_imx" target="_blank"&gt;https://hub.docker.com/repository/docker/fdsgfn/ubuntu21.04_imx&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Dec 2021 06:22:10 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2021-12-23T06:22:10Z</dc:date>
    <item>
      <title>support for docker on i.MX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/support-for-docker-on-i-MX8MP/m-p/1391103#M184914</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;We are trying to bring up docker on imx8m plus device, by including meta virtualization layer in the yocto image build, by following below steps:&lt;BR /&gt;1. Clone the meta-virtualization layer in sources directory&lt;BR /&gt;git clone &lt;A href="https://git.yoctoproject.org/git/meta-virtualization" target="_blank"&gt;https://git.yoctoproject.org/git/meta-virtualization&lt;/A&gt;&lt;/P&gt;&lt;P&gt;2. making changes in the “conf/bblayers.conf” by adding the following line&lt;BR /&gt;BBLAYERS += "${BSPDIR}/sources/meta-virtualization"&lt;/P&gt;&lt;P&gt;3. Add the following lines in “conf/local.conf” file&lt;BR /&gt;DISTRO_FEATURES_append = " virtualization"&lt;BR /&gt;IMAGE_INSTALL_append = " docker-ce".&lt;/P&gt;&lt;P&gt;4. Building the image using bitbake command.&lt;/P&gt;&lt;P&gt;But the docker command is not being recognized even after booting the board with the new image.&lt;/P&gt;&lt;P&gt;Could you please let us know whether including docker in yocto image is supported on imx8m plus device.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Dec 2021 05:32:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/support-for-docker-on-i-MX8MP/m-p/1391103#M184914</guid>
      <dc:creator>SachinMR</dc:creator>
      <dc:date>2021-12-23T05:32:41Z</dc:date>
    </item>
    <item>
      <title>Re: support for docker on i.MX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/support-for-docker-on-i-MX8MP/m-p/1391128#M184919</link>
      <description>&lt;P&gt;You can see this test docker image and it's readme:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://hub.docker.com/repository/docker/fdsgfn/ubuntu21.04_imx" target="_blank"&gt;https://hub.docker.com/repository/docker/fdsgfn/ubuntu21.04_imx&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Dec 2021 06:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/support-for-docker-on-i-MX8MP/m-p/1391128#M184919</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-12-23T06:22:10Z</dc:date>
    </item>
  </channel>
</rss>