<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Yocto imx6ulevk Build Error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-imx6ulevk-Build-Error/m-p/1390846#M184893</link>
    <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I am following the &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_self"&gt;NXP Guide&lt;/A&gt; for building an IMX6 EVK on Ubuntu.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have enough HDD space, I installed all of the necessary libraries yet I get one failure (Image Attached).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The error I receive happens at the end of build. It is an issue with c make which I have installed. I am running on Ubuntu 20.04 in a Virtual Box VM. Is there anything I can do?&lt;/P&gt;</description>
    <pubDate>Wed, 22 Dec 2021 15:55:25 GMT</pubDate>
    <dc:creator>MichaelBMiner</dc:creator>
    <dc:date>2021-12-22T15:55:25Z</dc:date>
    <item>
      <title>Yocto imx6ulevk Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-imx6ulevk-Build-Error/m-p/1390846#M184893</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I am following the &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_self"&gt;NXP Guide&lt;/A&gt; for building an IMX6 EVK on Ubuntu.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have enough HDD space, I installed all of the necessary libraries yet I get one failure (Image Attached).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The error I receive happens at the end of build. It is an issue with c make which I have installed. I am running on Ubuntu 20.04 in a Virtual Box VM. Is there anything I can do?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Dec 2021 15:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-imx6ulevk-Build-Error/m-p/1390846#M184893</guid>
      <dc:creator>MichaelBMiner</dc:creator>
      <dc:date>2021-12-22T15:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto imx6ulevk Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-imx6ulevk-Build-Error/m-p/1391389#M184952</link>
      <description>&lt;P&gt;Hello Michael,&lt;/P&gt;
&lt;P&gt;You don't show the error of the task, but i think the he CMake scripts for &lt;CODE&gt;cpsumon&lt;/CODE&gt; don't actually install the library anywhere, so the generated makefiles do not contain an &lt;CODE&gt;install&lt;/CODE&gt; target.&lt;/P&gt;
&lt;P&gt;Thus, when the &lt;CODE&gt;do_install&lt;/CODE&gt; task does &lt;CODE&gt;make install&lt;/CODE&gt;, you get the error from &lt;CODE&gt;make&lt;/CODE&gt; saying&lt;/P&gt;
&lt;P&gt;&lt;CODE&gt;make: *** No rule to make target 'install'.&lt;/CODE&gt;&lt;/P&gt;
&lt;P&gt;Then you need to run the sudo apt install cmake again and erase and burn again yocto.&lt;/P&gt;
&lt;P&gt;&lt;CODE&gt;&lt;/CODE&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;CODE&gt;&lt;/CODE&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Dec 2021 13:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-imx6ulevk-Build-Error/m-p/1391389#M184952</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-12-23T13:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto imx6ulevk Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-imx6ulevk-Build-Error/m-p/1391878#M185001</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I did install cmake and I now get two new errors that I have not investigated just yet.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 3396 tasks of which 0 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;virtual:native:/home/imx6yocto/Documents/imx-yocto-bsp/sources/poky/meta/recipes-devtools/python/python3-six_1.15.0.bb:do_fetch&lt;BR /&gt;Summary: There were 5 WARNING messages shown.&lt;BR /&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
      <pubDate>Fri, 24 Dec 2021 22:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-imx6ulevk-Build-Error/m-p/1391878#M185001</guid>
      <dc:creator>MichaelBMiner</dc:creator>
      <dc:date>2021-12-24T22:28:49Z</dc:date>
    </item>
  </channel>
</rss>