<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8 Mini: run microSD2 without reset pull-up in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-Mini-run-microSD2-without-reset-pull-up/m-p/1390694#M184873</link>
    <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I made a custom board based on IMX8MINI, but unfortunately, I did not pull up the RESET ball of uSD2.&lt;/P&gt;&lt;P&gt;I pulled up only BOOT_CFG[10], and BOOT_CFG[12] (all the rest are left float).&amp;nbsp; BOOT_MODE0 = 0, BOOT_MODE1 = 1. (Internal boot).&lt;/P&gt;&lt;P&gt;There is no activity at uSD2 lines at startup, the voltage at data lines - about 0.8V. (they are pulled-up t 0 3.3V). Also, there is no voltage at the dedicated vdd_uSD2 LDO output of the PMIC. As far as I understand - this is the only LDO that activates by software, but I can't see any activity on i2c lines at startup.&lt;/P&gt;&lt;P&gt;The USB works well, so I'm able to load and execute images, such as u-boot via the uuu tool. While loading SPL and U-boot - no voltage rise at LDO, so uSD2 doesn't work.&lt;/P&gt;&lt;P&gt;So, the questions are:&lt;/P&gt;&lt;P&gt;1. did I configure BOOT_CFG pins correctly?&lt;/P&gt;&lt;P&gt;2. is it mandatory to have an external pull-up on the uSD2_RESET ball?&lt;/P&gt;&lt;P&gt;3. Can I override this setting by PINMUX in the device tree (or somewhere else?)&lt;/P&gt;&lt;P&gt;4. Maybe I can somehow enable the uSD2 interface via u-boot shell?&lt;/P&gt;</description>
    <pubDate>Wed, 22 Dec 2021 09:25:34 GMT</pubDate>
    <dc:creator>Alex34</dc:creator>
    <dc:date>2021-12-22T09:25:34Z</dc:date>
    <item>
      <title>IMX8 Mini: run microSD2 without reset pull-up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-Mini-run-microSD2-without-reset-pull-up/m-p/1390694#M184873</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I made a custom board based on IMX8MINI, but unfortunately, I did not pull up the RESET ball of uSD2.&lt;/P&gt;&lt;P&gt;I pulled up only BOOT_CFG[10], and BOOT_CFG[12] (all the rest are left float).&amp;nbsp; BOOT_MODE0 = 0, BOOT_MODE1 = 1. (Internal boot).&lt;/P&gt;&lt;P&gt;There is no activity at uSD2 lines at startup, the voltage at data lines - about 0.8V. (they are pulled-up t 0 3.3V). Also, there is no voltage at the dedicated vdd_uSD2 LDO output of the PMIC. As far as I understand - this is the only LDO that activates by software, but I can't see any activity on i2c lines at startup.&lt;/P&gt;&lt;P&gt;The USB works well, so I'm able to load and execute images, such as u-boot via the uuu tool. While loading SPL and U-boot - no voltage rise at LDO, so uSD2 doesn't work.&lt;/P&gt;&lt;P&gt;So, the questions are:&lt;/P&gt;&lt;P&gt;1. did I configure BOOT_CFG pins correctly?&lt;/P&gt;&lt;P&gt;2. is it mandatory to have an external pull-up on the uSD2_RESET ball?&lt;/P&gt;&lt;P&gt;3. Can I override this setting by PINMUX in the device tree (or somewhere else?)&lt;/P&gt;&lt;P&gt;4. Maybe I can somehow enable the uSD2 interface via u-boot shell?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Dec 2021 09:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-Mini-run-microSD2-without-reset-pull-up/m-p/1390694#M184873</guid>
      <dc:creator>Alex34</dc:creator>
      <dc:date>2021-12-22T09:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 Mini: run microSD2 without reset pull-up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-Mini-run-microSD2-without-reset-pull-up/m-p/1390752#M184878</link>
      <description>&lt;P&gt;Hi Alex&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. for BOOT_CFG configuration one can look at p.11 SPF-31399 i.MX8M Mini EVK&lt;/P&gt;
&lt;P&gt;schematic&amp;nbsp;&lt;A id="docsAndSoftware_designResultTitle1_3" class="dtmcustomrulelink" href="https://www.nxp.com/webapp/Download?colCode=8MMINID4-EVK-DESIGNFILES" data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="i.MX 8M Mini Evaluation Kit DDR4 Design Files" target="_blank"&gt;i.MX 8M Mini Evaluation Kit DDR4 Design Files&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;2. it is mandatory as shown on p.6 schematic&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165973i558B8FB48C738110/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3.4.&amp;nbsp;&amp;nbsp; no&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 22 Dec 2021 10:44:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-Mini-run-microSD2-without-reset-pull-up/m-p/1390752#M184878</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-12-22T10:44:46Z</dc:date>
    </item>
  </channel>
</rss>