<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SABRE Lite powered by USB? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SABRE-Lite-powered-by-USB/m-p/235084#M18486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The adapter can provide 4A @5V, and as far as i know usb 2.0 only provides 500mA, so i dont think powering from usb is possible... btw,the datasheet says it requires &amp;gt;5W power just to turn on the board without any peripheral&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 27 Jan 2013 16:36:10 GMT</pubDate>
    <dc:creator>the_1080p_guy</dc:creator>
    <dc:date>2013-01-27T16:36:10Z</dc:date>
    <item>
      <title>SABRE Lite powered by USB?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SABRE-Lite-powered-by-USB/m-p/235083#M18485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a SABRE Lite and I was wondering if it was possible to power it via USB rather than the main adapter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 15:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SABRE-Lite-powered-by-USB/m-p/235083#M18485</guid>
      <dc:creator>patkelly18</dc:creator>
      <dc:date>2013-01-24T15:04:15Z</dc:date>
    </item>
    <item>
      <title>Re: SABRE Lite powered by USB?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SABRE-Lite-powered-by-USB/m-p/235084#M18486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The adapter can provide 4A @5V, and as far as i know usb 2.0 only provides 500mA, so i dont think powering from usb is possible... btw,the datasheet says it requires &amp;gt;5W power just to turn on the board without any peripheral&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 27 Jan 2013 16:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SABRE-Lite-powered-by-USB/m-p/235084#M18486</guid>
      <dc:creator>the_1080p_guy</dc:creator>
      <dc:date>2013-01-27T16:36:10Z</dc:date>
    </item>
    <item>
      <title>Re: SABRE Lite powered by USB?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SABRE-Lite-powered-by-USB/m-p/235085#M18487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the help. I found a work around of sorts. Although it can't be powered through the USB port like a lot of the lower powered boards. I was able to power it via a USB to Type M cable, so use my laptop and the existing power socket and it worked fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2013 16:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SABRE-Lite-powered-by-USB/m-p/235085#M18487</guid>
      <dc:creator>patkelly18</dc:creator>
      <dc:date>2013-01-30T16:33:14Z</dc:date>
    </item>
  </channel>
</rss>