<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Supporting single channel LPDDR4 on iMX8MP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1389312#M184721</link>
    <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Do you have any update on this case?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
    <pubDate>Mon, 20 Dec 2021 06:28:56 GMT</pubDate>
    <dc:creator>simonng</dc:creator>
    <dc:date>2021-12-20T06:28:56Z</dc:date>
    <item>
      <title>Supporting single channel LPDDR4 on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387065#M184457</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;Can the i.MX8MP processor support 200B LPDDR4 DRAM with only single channel?&lt;/P&gt;&lt;P&gt;If yes, is it channel A or channel B?&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 07:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387065#M184457</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2021-12-15T07:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: Supporting single channel LPDDR4 on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387201#M184488</link>
      <description>&lt;P&gt;Hi Simon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;in general it can be supported (channel A). Just for comparison one can look at&lt;/P&gt;
&lt;H3 class="media-flex-heading"&gt;&lt;A id="docsAndSoftware_designResultTitle1_2" class="dtmcustomrulelink" href="https://www.nxp.com/webapp/Download?colCode=8MMINILPD4-CPU2-DESIGNFILES" data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="i.MX 8M Mini LPDDR4 EVKB Compute Module Design Files" target="_blank"&gt;i.MX 8M Mini LPDDR4 EVKB Compute Module Design Files&lt;/A&gt;&lt;/H3&gt;
&lt;P&gt;and single channel&amp;nbsp; &lt;A id="docsAndSoftware_designResultTitle1_3" class="dtmcustomrulelink" href="https://www.nxp.com/webapp/Download?colCode=X-815LPD4-CPUCY-DF-SCH" data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="Design Files for an i.MX 8M Nano Compute Module with LPDDR4" target="_blank"&gt;Design Files for an i.MX 8M Nano Compute Module with LPDDR4&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 09:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387201#M184488</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-12-15T09:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: Supporting single channel LPDDR4 on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387773#M184545</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for your reply. I tried to set the single channel setting and run it on the 8MP EVKB (8MPLUSLPD4-EVK). Then I used the DDR Tool to run the Stress Test. But the test hang up. I noticed that the Col size is changed to 11 and the density per chip select is still 3072MB. I attached the ds file and RPA file. Can you help me to check this problem?&lt;/P&gt;&lt;P&gt;Here is the log:&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;ARM clock(CA53) rate: 1800MHz&lt;BR /&gt;DDR Clock: 2000MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;DDR type is LPDDR4&lt;BR /&gt;Data width: 16, bank num: 8&lt;BR /&gt;Row size: 17, col size: 11&lt;/P&gt;&lt;P&gt;Note: though not necessarily in error, it is normally unusual&lt;BR /&gt;to have a number of column address bits exceed 10. It is recommended&lt;BR /&gt;to double check the DRAM data sheet to ensure the correct column count and&lt;BR /&gt;to set unused column address bits in registers ADDRMAP3 and ADDRMAP4 to 0xF&lt;BR /&gt;or else the there will be a miscalculation of the total density&lt;/P&gt;&lt;P&gt;Two chip selects are used&lt;BR /&gt;Number of DDR controllers used on the SoC: 1&lt;BR /&gt;Density per chip select: 3072MB&lt;BR /&gt;Density per controller is: 6144MB&lt;BR /&gt;Total density detected on the board is: 6144MB&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;MX8M-plus: Cortex-A53 is found&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;============ Step 1: DDRPHY Training... ============&lt;BR /&gt;---DDR 1D-Training @2000Mhz...&lt;BR /&gt;[Process] End of CA training&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;[Process] End of read DQ deskew training&lt;BR /&gt;[Process] End of MPR read delay center optimization&lt;BR /&gt;[Process] End of Write Leveling coarse delay&lt;BR /&gt;[Process] End of write delay center optimization&lt;BR /&gt;[Process] End of read delay center optimization&lt;BR /&gt;[Process] End of max read latency training&lt;BR /&gt;[Result] PASS&lt;BR /&gt;---DDR 1D-Training @200Mhz...&lt;BR /&gt;[Process] End of CA training&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;[Process] End of MPR read delay center optimization&lt;BR /&gt;[Process] End of Write Leveling coarse delay&lt;BR /&gt;[Process] End of write delay center optimization&lt;BR /&gt;[Process] End of read delay center optimization&lt;BR /&gt;[Process] End of max read latency training&lt;BR /&gt;[Result] PASS&lt;BR /&gt;---DDR 1D-Training @50Mhz...&lt;BR /&gt;[Process] End of CA training&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;[Process] End of MPR read delay center optimization&lt;BR /&gt;[Process] End of Write Leveling coarse delay&lt;BR /&gt;[Process] End of write delay center optimization&lt;BR /&gt;[Process] End of read delay center optimization&lt;BR /&gt;[Process] End of max read latency training&lt;BR /&gt;[Result] PASS&lt;BR /&gt;---DDR 2D-Training @2000Mhz...&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of 2D write delay/voltage center optimization&lt;BR /&gt;[Process] End of 2D read delay/voltage center optimization&lt;BR /&gt;[Result] PASS&lt;/P&gt;&lt;P&gt;============ Step 2: DDR memory accessing... ============&lt;BR /&gt;Verifying DDR frequency point0@2000MHz.......Pass&lt;BR /&gt;Verifying DDR frequency point1@200MHz.......Pass&lt;BR /&gt;Verifying DDR frequency point2@50MHz.......Pass&lt;BR /&gt;[Result] OK&lt;/P&gt;&lt;P&gt;============ Step 3: DDR parameters processing... ============&lt;BR /&gt;[Result] Done&lt;/P&gt;&lt;P&gt;Success: DDR Calibration completed!!!&lt;BR /&gt;DDR Stress Test Iteration 1&lt;BR /&gt;--------------------------------&lt;BR /&gt;--Running DDR test on region 1--&lt;BR /&gt;--------------------------------&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 03:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387773#M184545</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2021-12-16T03:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: Supporting single channel LPDDR4 on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1389312#M184721</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Do you have any update on this case?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Mon, 20 Dec 2021 06:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1389312#M184721</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2021-12-20T06:28:56Z</dc:date>
    </item>
    <item>
      <title>Re: Supporting single channel LPDDR4 on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1392784#M185129</link>
      <description>&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;Are you still looking at this issue? Please help me to follow up.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 29 Dec 2021 02:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1392784#M185129</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2021-12-29T02:16:14Z</dc:date>
    </item>
  </channel>
</rss>