<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MSCALE-SECO FW version issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-SECO-FW-version-issue/m-p/1388819#M184648</link>
    <description>&lt;P&gt;I discovered the problem, I was on the wrong UART (I was on SCU UART, not UART0).&lt;/P&gt;&lt;P&gt;Note: even with a new board without SCFW or any software, the DDR tools is working correctly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 17 Dec 2021 12:59:09 GMT</pubDate>
    <dc:creator>PBR</dc:creator>
    <dc:date>2021-12-17T12:59:09Z</dc:date>
    <item>
      <title>MSCALE-SECO FW version issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-SECO-FW-version-issue/m-p/1385746#M184363</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have to check the DDR4 of my new custom board with a IMX8QXP-C0.&lt;/P&gt;&lt;P&gt;I am using MSCALE software: mx8_ddr_stress_test_ER14_installation.zip which seems the latest.&lt;/P&gt;&lt;P&gt;This one is working on my IMX8QXP EVM board but not on my custom board.&lt;/P&gt;&lt;P&gt;The IMX8QXP-C0 on my board has no installed firmware and is configured in serial boot mode.&lt;/P&gt;&lt;P&gt;Please see me attached log files: one with my EVM board and one with my custom board. There are really different. Why?&lt;/P&gt;&lt;P&gt;On the custom board (DDR-UBR.log), it is written at the end:&lt;/P&gt;&lt;P&gt;"Incorrect SECO FW version 2.5.4 (2.6.0 or later required)"&lt;/P&gt;&lt;P&gt;The Seco FW is given by the Mscale, am I right? So does it mean my Mscale is not the latest? Do you have a new one?&lt;/P&gt;&lt;P&gt;Or do I need to download a Seco FW prior using Mscale? With uuu?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 15:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-SECO-FW-version-issue/m-p/1385746#M184363</guid>
      <dc:creator>PBR</dc:creator>
      <dc:date>2021-12-13T15:34:07Z</dc:date>
    </item>
    <item>
      <title>Re: MSCALE-SECO FW version issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-SECO-FW-version-issue/m-p/1386821#M184437</link>
      <description>&lt;P&gt;pls refer to the link as below:&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Incorrect-SCFO-FW-version-message-when-using-DDR-Stress-Test/m-p/1150080" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Incorrect-SCFO-FW-version-message-when-using-DDR-Stress-Test/m-p/1150080&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 02:26:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-SECO-FW-version-issue/m-p/1386821#M184437</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-12-15T02:26:45Z</dc:date>
    </item>
    <item>
      <title>Re: MSCALE-SECO FW version issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-SECO-FW-version-issue/m-p/1388819#M184648</link>
      <description>&lt;P&gt;I discovered the problem, I was on the wrong UART (I was on SCU UART, not UART0).&lt;/P&gt;&lt;P&gt;Note: even with a new board without SCFW or any software, the DDR tools is working correctly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 12:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-SECO-FW-version-issue/m-p/1388819#M184648</guid>
      <dc:creator>PBR</dc:creator>
      <dc:date>2021-12-17T12:59:09Z</dc:date>
    </item>
  </channel>
</rss>