<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: SEMC SRAM interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1388796#M184645</link>
    <description>&lt;P&gt;Yes, it is possible to use upper address pins (A16 and higher) as GPIOs when &lt;BR /&gt;SEMC operates in SRAM mode. Just configure these pins as GPIOs in IOMUXC.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
    <pubDate>Fri, 17 Dec 2021 11:22:37 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2021-12-17T11:22:37Z</dc:date>
    <item>
      <title>SEMC SRAM interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1382578#M184069</link>
      <description>&lt;P&gt;product: I.mxrt 1170 series&lt;/P&gt;&lt;P&gt;For the SRAM write/read in SYNC mode (ADMUX), just wonder is it possible to mask the higher address bit, A[M : 16], means not to use and free up my address pin, so that I can connect them extra GPIOs.&lt;/P&gt;&lt;P&gt;My SRAM application only need A0-15.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SEMC SRAM masking.jpg" style="width: 667px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/164317iACBABE9C156CE10F/image-size/large?v=v2&amp;amp;px=999" role="button" title="SEMC SRAM masking.jpg" alt="SEMC SRAM masking.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 10:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1382578#M184069</guid>
      <dc:creator>ShiXiang</dc:creator>
      <dc:date>2021-12-07T10:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1384467#M184225</link>
      <description>&lt;P&gt;Can the software call function/register support on masking or is the software/register adjustable? For masking the higher address bit, A[M : 16], while using&amp;nbsp;SRAM write/read in SYNC mode (ADMUX) . Thank you.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Dec 2021 02:53:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1384467#M184225</guid>
      <dc:creator>ShiXiang</dc:creator>
      <dc:date>2021-12-10T02:53:32Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1387690#M184536</link>
      <description>&lt;P&gt;No reply yet, re-post to I.MX RT page.&lt;/P&gt;&lt;P&gt;Please close this question, thank you.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 01:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1387690#M184536</guid>
      <dc:creator>ShiXiang</dc:creator>
      <dc:date>2021-12-16T01:42:12Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1388796#M184645</link>
      <description>&lt;P&gt;Yes, it is possible to use upper address pins (A16 and higher) as GPIOs when &lt;BR /&gt;SEMC operates in SRAM mode. Just configure these pins as GPIOs in IOMUXC.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 11:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SEMC-SRAM-interface/m-p/1388796#M184645</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-12-17T11:22:37Z</dc:date>
    </item>
  </channel>
</rss>