<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8Mplus USB1_VBUS characteristics in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8Mplus-USB1-VBUS-characteristics/m-p/1388624#M184614</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;in my design, USB1 is used as device. For this reason, VBUS-sensing is reqired.&lt;/P&gt;&lt;P&gt;I cannot find the characteristics of USB1_VBUS in the datahsheet. Is it possible to sense VBUS using a resistive voltage divider? In this case, a small current could be injected into this port, if VDD_USB_3P3 is down.&lt;/P&gt;&lt;P&gt;Or do i need to treat USB1_VBUS as 3.3V-port with special function, requiring a external logic gate or comparator?&lt;/P&gt;</description>
    <pubDate>Fri, 17 Dec 2021 07:36:26 GMT</pubDate>
    <dc:creator>max123</dc:creator>
    <dc:date>2021-12-17T07:36:26Z</dc:date>
    <item>
      <title>i.MX8Mplus USB1_VBUS characteristics</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8Mplus-USB1-VBUS-characteristics/m-p/1388624#M184614</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;in my design, USB1 is used as device. For this reason, VBUS-sensing is reqired.&lt;/P&gt;&lt;P&gt;I cannot find the characteristics of USB1_VBUS in the datahsheet. Is it possible to sense VBUS using a resistive voltage divider? In this case, a small current could be injected into this port, if VDD_USB_3P3 is down.&lt;/P&gt;&lt;P&gt;Or do i need to treat USB1_VBUS as 3.3V-port with special function, requiring a external logic gate or comparator?&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 07:36:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8Mplus-USB1-VBUS-characteristics/m-p/1388624#M184614</guid>
      <dc:creator>max123</dc:creator>
      <dc:date>2021-12-17T07:36:26Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8Mplus USB1_VBUS characteristics</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8Mplus-USB1-VBUS-characteristics/m-p/1390080#M184795</link>
      <description>&lt;P&gt;The USBx_VBUS pin cannot directly connect to 5 V VBUS voltage on the USB2.0 link, each&lt;BR /&gt;USBx_VBUS pin must be isolated by an external 30 K 1% precision resistor if connects to 5 V VBUS.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Dec 2021 10:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8Mplus-USB1-VBUS-characteristics/m-p/1390080#M184795</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-12-21T10:05:08Z</dc:date>
    </item>
  </channel>
</rss>