<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックkernel install - stand alone</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/kernel-install-stand-alone/m-p/1388198#M184585</link>
    <description>&lt;P&gt;I built the kernel with poky-linux cross compiler and I got Image, Image.gz, install.sh, Makefile and dts in arch/arm64/boot of HOST PC.&lt;/P&gt;&lt;P&gt;But I don't know how to do next. I want to install the cross-compiled kernel to target board from host pc.&lt;/P&gt;&lt;P&gt;The target board is booted from internal eMMC.&lt;/P&gt;&lt;P&gt;Do I copies the all files to /boot directory of target board and do 'make install' or else?&lt;/P&gt;&lt;P&gt;I don't know how to adjust it properly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additionally, I wonder that the RGMII version of imx8mq-evk. Is it higer than v2.0?&lt;/P&gt;</description>
    <pubDate>Thu, 16 Dec 2021 14:32:08 GMT</pubDate>
    <dc:creator>CHOIzee</dc:creator>
    <dc:date>2021-12-16T14:32:08Z</dc:date>
    <item>
      <title>kernel install - stand alone</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-install-stand-alone/m-p/1388198#M184585</link>
      <description>&lt;P&gt;I built the kernel with poky-linux cross compiler and I got Image, Image.gz, install.sh, Makefile and dts in arch/arm64/boot of HOST PC.&lt;/P&gt;&lt;P&gt;But I don't know how to do next. I want to install the cross-compiled kernel to target board from host pc.&lt;/P&gt;&lt;P&gt;The target board is booted from internal eMMC.&lt;/P&gt;&lt;P&gt;Do I copies the all files to /boot directory of target board and do 'make install' or else?&lt;/P&gt;&lt;P&gt;I don't know how to adjust it properly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additionally, I wonder that the RGMII version of imx8mq-evk. Is it higer than v2.0?&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 14:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-install-stand-alone/m-p/1388198#M184585</guid>
      <dc:creator>CHOIzee</dc:creator>
      <dc:date>2021-12-16T14:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: kernel install - stand alone</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-install-stand-alone/m-p/1388844#M184651</link>
      <description>&lt;P&gt;Hello&amp;nbsp; CHOLzee,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Download the latest yocto BSP documentation, you can build the uboot, dtb, and kernel separately, it comes with the toolchain for crosscompiling, and yes the RGMII is higher than 2.0.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 14:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-install-stand-alone/m-p/1388844#M184651</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-12-17T14:24:31Z</dc:date>
    </item>
  </channel>
</rss>