<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to write to i.mx8mn eFuses from userspace</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-write-to-i-mx8mn-eFuses-from-userspace/m-p/1387349#M184510</link>
    <description>&lt;P&gt;Question in the title. Having a hard time managing to write to eFuses on the i.mx8mn from userspace.&amp;nbsp; Using fuse in u-boot works great though so no problems there. The secure boot guide&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Steps-to-enable-secure-boot-in-i-MX8M-Nano/ta-p/1246417" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Steps-to-enable-secure-boot-in-i-MX8M-Nano/ta-p/1246417&lt;/A&gt;&amp;nbsp;helps little. This talks about how to burn efuses on the i.mx8mn:&amp;nbsp;&lt;A href="https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/" target="_blank"&gt;https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/&lt;/A&gt;. I do however not see a clear way to get access to the SCFW API in a program or elsewhere. I am not aware of what the "SC_R_SYSTEM" resource is so that explanation is not sufficient. An elaboration of how one can access this API from a C/cpp program would be greatly appreciated&lt;/P&gt;</description>
    <pubDate>Wed, 15 Dec 2021 13:56:55 GMT</pubDate>
    <dc:creator>KjetilSekseKristiansen</dc:creator>
    <dc:date>2021-12-15T13:56:55Z</dc:date>
    <item>
      <title>How to write to i.mx8mn eFuses from userspace</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-write-to-i-mx8mn-eFuses-from-userspace/m-p/1387349#M184510</link>
      <description>&lt;P&gt;Question in the title. Having a hard time managing to write to eFuses on the i.mx8mn from userspace.&amp;nbsp; Using fuse in u-boot works great though so no problems there. The secure boot guide&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Steps-to-enable-secure-boot-in-i-MX8M-Nano/ta-p/1246417" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Steps-to-enable-secure-boot-in-i-MX8M-Nano/ta-p/1246417&lt;/A&gt;&amp;nbsp;helps little. This talks about how to burn efuses on the i.mx8mn:&amp;nbsp;&lt;A href="https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/" target="_blank"&gt;https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/&lt;/A&gt;. I do however not see a clear way to get access to the SCFW API in a program or elsewhere. I am not aware of what the "SC_R_SYSTEM" resource is so that explanation is not sufficient. An elaboration of how one can access this API from a C/cpp program would be greatly appreciated&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 13:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-write-to-i-mx8mn-eFuses-from-userspace/m-p/1387349#M184510</guid>
      <dc:creator>KjetilSekseKristiansen</dc:creator>
      <dc:date>2021-12-15T13:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: How to write to i.mx8mn eFuses from userspace</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-write-to-i-mx8mn-eFuses-from-userspace/m-p/1387645#M184528</link>
      <description>&lt;P&gt;Hi Kjetil&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try solution provided on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/OCOTP-write-support-on-i-mx8m/m-p/825028?commentID=1161432&amp;amp;et=watches.email.thread#comment" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/OCOTP-write-support-on-i-mx8m/m-p/825028?commentID=1161432&amp;amp;et=watches.email.thread#comment&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 23:46:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-write-to-i-mx8mn-eFuses-from-userspace/m-p/1387645#M184528</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-12-15T23:46:10Z</dc:date>
    </item>
  </channel>
</rss>