<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mm-evk question: cannot flash bootloader via uuu tool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1386887#M184441</link>
    <description>&lt;P&gt;Hi NXP community:&lt;/P&gt;&lt;P&gt;In recent days I am trying to burn the Yocto image in my imx8-mini board and I got an error when I was flashing the bootloader into the board as I said.&lt;/P&gt;&lt;P&gt;I referenced this document to generate my imx-robot-core-rt image strictly:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B3%E5%8F%B0-i-MX-Robot-Platform/ta-p/1198619" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B3%E5%8F%B0-i-MX-Robot-Platform/ta-p/1198619&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And here is the error log:&lt;/P&gt;&lt;P&gt;==============================================================================&lt;/P&gt;&lt;P&gt;PS D:\uuu&amp;gt; uuu.exe -V -b emmc D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.165-0-ge10b026&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt;Pctl Chip Vid Pid BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt;SDPS: MX28 0x15a2 0x004f&lt;BR /&gt;SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt;SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014a&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014b&lt;BR /&gt;SDP: MX7D 0x15a2 0x0076&lt;BR /&gt;SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt;SDP: MX6D 0x15a2 0x0061&lt;BR /&gt;SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt;SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt;SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt;SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt;SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt;SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt;SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt;SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt;SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt;SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt;FBK: 0x066f 0x9afe&lt;BR /&gt;FBK: 0x066f 0x9bff&lt;BR /&gt;FB: 0x0525 0xa4a5&lt;BR /&gt;FB: 0x18d1 0x0d02&lt;BR /&gt;FB: 0x3016 0x0001&lt;/P&gt;&lt;P&gt;Run built-in script:&lt;/P&gt;&lt;P&gt;uuu_version 1.2.39&lt;/P&gt;&lt;P&gt;# @_flash.bin | bootloader&lt;BR /&gt;# @_image [_flash.bin] | image burn to emmc, default is the same as bootloader&lt;/P&gt;&lt;P&gt;# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ&lt;BR /&gt;SDP: boot -f D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk&lt;/P&gt;&lt;P&gt;# This command will be run when ROM support stream mode&lt;BR /&gt;# i.MX8QXP, i.MX8QM&lt;BR /&gt;SDPS: boot -f D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# SDPU will be deprecated. please use SDPV instead of SDPU&lt;BR /&gt;# {&lt;BR /&gt;SDPU: delay 1000&lt;BR /&gt;SDPU: write -f D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk -offset 0x57c00&lt;BR /&gt;SDPU: jump&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# if (SPL support SDPV)&lt;BR /&gt;# {&lt;BR /&gt;SDPV: delay 1000&lt;BR /&gt;SDPV: write -f D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk -skipspl&lt;BR /&gt;SDPV: jump&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;FB: ucmd mmc dev ${emmc_dev}&lt;BR /&gt;FB: flash bootloader D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk&lt;BR /&gt;FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;&lt;BR /&gt;FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0&lt;BR /&gt;FB: Done&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 1:10&lt;BR /&gt;1:10&amp;gt;Start Cmd:FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;1:10&amp;gt;Okay (0.004s)&lt;BR /&gt;1:10&amp;gt;Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;1:10&amp;gt;Okay (0.004s)&lt;BR /&gt;1:10&amp;gt;Start Cmd:FB: ucmd mmc dev ${emmc_dev}&lt;BR /&gt;1:10&amp;gt;Fail (0.006s)&lt;/P&gt;&lt;P&gt;==============================================================================&lt;/P&gt;&lt;P&gt;Any idea about it? Thanks a lot!&lt;/P&gt;</description>
    <pubDate>Wed, 15 Dec 2021 03:58:08 GMT</pubDate>
    <dc:creator>bitterblossom5486</dc:creator>
    <dc:date>2021-12-15T03:58:08Z</dc:date>
    <item>
      <title>imx8mm-evk question: cannot flash bootloader via uuu tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1386887#M184441</link>
      <description>&lt;P&gt;Hi NXP community:&lt;/P&gt;&lt;P&gt;In recent days I am trying to burn the Yocto image in my imx8-mini board and I got an error when I was flashing the bootloader into the board as I said.&lt;/P&gt;&lt;P&gt;I referenced this document to generate my imx-robot-core-rt image strictly:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B3%E5%8F%B0-i-MX-Robot-Platform/ta-p/1198619" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B3%E5%8F%B0-i-MX-Robot-Platform/ta-p/1198619&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And here is the error log:&lt;/P&gt;&lt;P&gt;==============================================================================&lt;/P&gt;&lt;P&gt;PS D:\uuu&amp;gt; uuu.exe -V -b emmc D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.165-0-ge10b026&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt;Pctl Chip Vid Pid BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt;SDPS: MX28 0x15a2 0x004f&lt;BR /&gt;SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt;SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014a&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014b&lt;BR /&gt;SDP: MX7D 0x15a2 0x0076&lt;BR /&gt;SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt;SDP: MX6D 0x15a2 0x0061&lt;BR /&gt;SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt;SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt;SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt;SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt;SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt;SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt;SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt;SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt;SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt;SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt;FBK: 0x066f 0x9afe&lt;BR /&gt;FBK: 0x066f 0x9bff&lt;BR /&gt;FB: 0x0525 0xa4a5&lt;BR /&gt;FB: 0x18d1 0x0d02&lt;BR /&gt;FB: 0x3016 0x0001&lt;/P&gt;&lt;P&gt;Run built-in script:&lt;/P&gt;&lt;P&gt;uuu_version 1.2.39&lt;/P&gt;&lt;P&gt;# @_flash.bin | bootloader&lt;BR /&gt;# @_image [_flash.bin] | image burn to emmc, default is the same as bootloader&lt;/P&gt;&lt;P&gt;# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ&lt;BR /&gt;SDP: boot -f D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk&lt;/P&gt;&lt;P&gt;# This command will be run when ROM support stream mode&lt;BR /&gt;# i.MX8QXP, i.MX8QM&lt;BR /&gt;SDPS: boot -f D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# SDPU will be deprecated. please use SDPV instead of SDPU&lt;BR /&gt;# {&lt;BR /&gt;SDPU: delay 1000&lt;BR /&gt;SDPU: write -f D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk -offset 0x57c00&lt;BR /&gt;SDPU: jump&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# if (SPL support SDPV)&lt;BR /&gt;# {&lt;BR /&gt;SDPV: delay 1000&lt;BR /&gt;SDPV: write -f D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk -skipspl&lt;BR /&gt;SDPV: jump&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;FB: ucmd mmc dev ${emmc_dev}&lt;BR /&gt;FB: flash bootloader D:\uuu\imx-boot-imx8mm-ddr4-evk-sd.bin-flash_ddr4_evk&lt;BR /&gt;FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;&lt;BR /&gt;FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0&lt;BR /&gt;FB: Done&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 1:10&lt;BR /&gt;1:10&amp;gt;Start Cmd:FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;1:10&amp;gt;Okay (0.004s)&lt;BR /&gt;1:10&amp;gt;Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;1:10&amp;gt;Okay (0.004s)&lt;BR /&gt;1:10&amp;gt;Start Cmd:FB: ucmd mmc dev ${emmc_dev}&lt;BR /&gt;1:10&amp;gt;Fail (0.006s)&lt;/P&gt;&lt;P&gt;==============================================================================&lt;/P&gt;&lt;P&gt;Any idea about it? Thanks a lot!&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 03:58:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1386887#M184441</guid>
      <dc:creator>bitterblossom5486</dc:creator>
      <dc:date>2021-12-15T03:58:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm-evk question: cannot flash bootloader via uuu tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1386889#M184442</link>
      <description>&lt;P&gt;And the uuu tool I used is the latest version.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 03:59:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1386889#M184442</guid>
      <dc:creator>bitterblossom5486</dc:creator>
      <dc:date>2021-12-15T03:59:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm-evk question: cannot flash bootloader via uuu tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1386968#M184449</link>
      <description>&lt;P&gt;&amp;nbsp;I read the tutorial of uuu again: &lt;A href="https://github.com/NXPmicro/mfgtools" target="_blank"&gt;https://github.com/NXPmicro/mfgtools&lt;/A&gt;&amp;nbsp;. Should I &lt;EM&gt;&lt;STRONG&gt;download&lt;/STRONG&gt; &lt;/EM&gt;a bootloader or &lt;EM&gt;&lt;STRONG&gt;flash&lt;/STRONG&gt; &lt;/EM&gt;it? I'm kind of confused 'cuz I cannot figure out these two concepts now sry for that. Did I use the incorrect bootloader flashing command? Anyway, the tutorial said that the bootloader should enable fastboot, then should I enable that mode manually?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 06:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1386968#M184449</guid>
      <dc:creator>bitterblossom5486</dc:creator>
      <dc:date>2021-12-15T06:09:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm-evk question: cannot flash bootloader via uuu tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1387051#M184455</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I connected one more USB-RS232 cable to the baseboard, then I got more info from the serial port. Hopefully that will be helpful:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;==============================================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2021.04-lf_v2021.04+g1c0116f3da (Sep 06 2021 - 08:48:23 +0000)&lt;BR /&gt;power_bd71837_init&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 2400MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from USB SDP&lt;BR /&gt;SDP: initialize...&lt;BR /&gt;SDP: handle requests...&lt;BR /&gt;Downloading file of size 3451152 to 0x40400000... done&lt;BR /&gt;Jumping to header at 0x40400000&lt;BR /&gt;Header Tag is not an IMX image&lt;BR /&gt;Found header at 0x4042a5a0&lt;BR /&gt;NOTICE: BL31: v2.4(release):lf-5.10.52-2.1.0-rc1-39-gbb4957067&lt;BR /&gt;NOTICE: BL31: Built : 04:45:39, Sep 8 2021&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2021.04-lf_v2021.04+g1c0116f3da (Sep 06 2021 - 08:48:23 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 44C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM DDR4 EVK with CYW43455 WIFI/BT board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;tcpc_init: Can't find device id=0x52&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-19&lt;BR /&gt;NAND: 0 MiB&lt;BR /&gt;MMC: FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... MMC: no card present&lt;BR /&gt;*** Warning - No block device, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;mxs_video lcdif@32e00000: failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;/P&gt;&lt;P&gt;[0] lcdif@32e00000, video&lt;BR /&gt;[1] mipi_dsi@32e10000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;mxs_video lcdif@32e00000: failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;SEC0: RNG instantiated&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF bb49570&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net: Could not get PHY for FEC0: addr 0&lt;BR /&gt;Could not get PHY for FEC0: addr 0&lt;BR /&gt;No ethernet found.&lt;/P&gt;&lt;P&gt;Fastboot: Normal&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;*** Warning - Use default environment for mfgtools&lt;BR /&gt;, using default environment&lt;/P&gt;&lt;P&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;## Checking Image at 43800000 ...&lt;BR /&gt;Unknown image format!&lt;BR /&gt;Run fastboot ...&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;MMC: no card present&lt;BR /&gt;MMC card init failed!&lt;BR /&gt;MMC: no card present&lt;BR /&gt;** Block device MMC 1 not supported&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;MMC Device 2 not found&lt;BR /&gt;invalid mmc device 2&lt;BR /&gt;MMC Device 2 not found&lt;BR /&gt;no mmc device at slot 2&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 07:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1387051#M184455</guid>
      <dc:creator>bitterblossom5486</dc:creator>
      <dc:date>2021-12-15T07:27:31Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm-evk question: cannot flash bootloader via uuu tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1387101#M184463</link>
      <description>&lt;P&gt;Are you using NXP i.MX8MM EVK board? Which version BSP are you using, are you using the demo images or the images you build yourself?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 08:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1387101#M184463</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-12-15T08:10:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm-evk question: cannot flash bootloader via uuu tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1387191#M184486</link>
      <description>&lt;P&gt;Well, neither demo image nor self-made image is not applicable. The processor is imx8mm but the baseboard is not.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 09:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1387191#M184486</guid>
      <dc:creator>bitterblossom5486</dc:creator>
      <dc:date>2021-12-15T09:24:29Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm-evk question: cannot flash bootloader via uuu tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1387977#M184560</link>
      <description>&lt;P&gt;Are the board you designed yourself? If yes, you need to do porting BSP first.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 08:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1387977#M184560</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-12-16T08:46:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm-evk question: cannot flash bootloader via uuu tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1388097#M184572</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;i.MX8MM has two type of evk board.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. i.MX8MM + LPDDR4 + emmc&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. i.MX8MM + DDR4&amp;nbsp; + nand&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which one you are using?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are using&amp;nbsp;i.MX8MM + DDR4&amp;nbsp; + nand&amp;nbsp; evk, it has no emmc.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;That is why the error output "&lt;SPAN&gt;invalid mmc device 2&lt;/SPAN&gt;" and you cannot flash to emmc.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;U-Boot 2021.04-lf_v2021.04+g1c0116f3da (Sep 06 2021 - 08:48:23 +0000)&lt;/P&gt;
&lt;P&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 44C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM DDR4 EVK with CYW43455 WIFI/BT board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;tcpc_init: Can't find device id=0x52&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 11:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-evk-question-cannot-flash-bootloader-via-uuu-tool/m-p/1388097#M184572</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2021-12-16T11:09:04Z</dc:date>
    </item>
  </channel>
</rss>