<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Yocto project image not booting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-image-not-booting/m-p/1386778#M184430</link>
    <description>&lt;P&gt;Hi Luca&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for sabrelite board one can look at boundary devices tutorial&lt;/P&gt;
&lt;P&gt;&lt;A href="https://boundarydevices.com/programming-emmc-on-i-mx6/" target="_blank"&gt;https://boundarydevices.com/programming-emmc-on-i-mx6/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Wed, 15 Dec 2021 00:37:22 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2021-12-15T00:37:22Z</dc:date>
    <item>
      <title>Yocto project image not booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-image-not-booting/m-p/1386536#M184419</link>
      <description>&lt;P&gt;I could build an image for imx6 sabrelite following Yocto tutorial.&lt;/P&gt;&lt;P&gt;Here is the log&lt;/P&gt;&lt;P&gt;NOTE: Your conf/bblayers.conf has been automatically updated.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.36.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "ubuntu-16.04"&lt;BR /&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;BR /&gt;MACHINE = "imx6dlsabresd"&lt;BR /&gt;DISTRO = "fsl-imx-fb"&lt;BR /&gt;DISTRO_VERSION = "4.9.88-2.0.0"&lt;BR /&gt;TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa9"&lt;BR /&gt;TARGET_FPU = "hard"&lt;BR /&gt;meta&lt;BR /&gt;meta-poky = "HEAD:0ec241873367e18f5371a3ad9aca1e2801dcd4ee"&lt;BR /&gt;meta-oe&lt;BR /&gt;meta-multimedia = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-freescale = "HEAD:49ac225a38f6d84519798e3264f2e4d19b84f70a"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:1d6d5961dbf82624b28bb318b4950a64abc31d12"&lt;BR /&gt;meta-freescale-distro = "HEAD:0ec6d7e206705702b5b534611754de0787f92b72"&lt;BR /&gt;meta-bsp&lt;BR /&gt;meta-sdk = "HEAD:d65692ecb3a4136fc1cc137152634e8633ddb3c6"&lt;BR /&gt;meta-browser = "HEAD:d6f9aed41c73b75a97d71bff060b03a66ee087b1"&lt;BR /&gt;meta-gnome&lt;BR /&gt;meta-networking&lt;BR /&gt;meta-python&lt;BR /&gt;meta-filesystems = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-qt5 = "HEAD:32bb7d18a08d1c48873d7ab6332d4cc3815a4dff"&lt;/P&gt;&lt;P&gt;I flashed the generated image on a 4Gb MMC following the instruction using dd command:&lt;/P&gt;&lt;P&gt;sudo dd if=&amp;lt;iamge name&amp;gt;.sdcard of=/dev/sd&amp;lt;partition&amp;gt; bs=1M conv=fsync&lt;/P&gt;&lt;P&gt;I had on my sd card two partition&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;a 8Mb of the boot is fat16&lt;/LI&gt;&lt;LI&gt;the remaining is for root and is ext4&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;when i try to boot this is the u-boot output&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot 2020.10-53068-ga173e0c8f7 (Nov 18 2021 - 09:25:14 -0800), Build: jenkins-uboot_v2020.10-166&lt;/P&gt;&lt;P&gt;CPU: i.MX6Q rev1.2 at 792 MHz&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Boundary Devices i.MX6 Quad Nitrogen6x Board&lt;BR /&gt;Board: sabrelite&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from SPIFlash...&lt;BR /&gt;SF: Detected sst25vf016b with page size 256 Bytes, erase size 4 KiB, total 2 MiB&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;BR /&gt;U-Boot 2020.10-53068-ga173e0c8f7 (Nov 18 2021 - 09:25:14 -0800), Build: jenkins-uboot_v2020.10-166x720M@60 (1280x720)&lt;BR /&gt;In: serial&lt;BR /&gt;CPU: i.MX6Q rev1.2 at 792 MHz&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Boundary Devices i.MX6 Quad Nitrogen6x Board&lt;BR /&gt;Board: sabrelite_ether&lt;BR /&gt;I2C: readyto stop autoboot: 0&lt;BR /&gt;DRAM: 1 GiB present&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from SPIFlash...&lt;BR /&gt;SF: Detected sst25vf016b with page size 256 Bytes, erase size 4 KiB, total 2 MiB&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;BR /&gt;starting USB...&lt;BR /&gt;Display: hdmi:1280x720M@60 (1280x720)d&lt;BR /&gt;In: serial00: USB EHCI 1.00&lt;BR /&gt;Out: serialusb@2184200 for devices... 2 USB Device(s) found&lt;BR /&gt;Err: serialng usb for storage devices... 0 Storage Device(s) found&lt;BR /&gt;Net: Micrel ksz9021 at 6hernet devices... 0 Ethernet Device(s) found&lt;BR /&gt;FEC [PRIME], usb_ether&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;Scanning mmc 0:1...&lt;BR /&gt;MMC: no card present&lt;BR /&gt;mmc_init: -123, time 2&lt;BR /&gt;Cannot probe SATA device 0 (err=-19)&lt;BR /&gt;starting USB...&lt;BR /&gt;Bus usb@2184000: usb dr_mode not found&lt;BR /&gt;Bus usb@2184200: USB EHCI 1.00&lt;BR /&gt;scanning bus usb@2184200 for devices... 2 USB Device(s) found&lt;BR /&gt;scanning usb for storage devices... 0 Storage Device(s) found&lt;BR /&gt;scanning usb for ethernet devices... 0 Ethernet Device(s) found&lt;/P&gt;&lt;P&gt;Device 0: unknown device&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I list partition 1 and 2 of MMC 0 which are boot and root partition, but if i try to access partition 0 of mmc 0 i got unknown fs result.&lt;/P&gt;&lt;P&gt;It seems the parttion 0 is not existing and is the one the device is trying to boot, did I miss something?&lt;/P&gt;&lt;P&gt;Thanks in advance for your answers&lt;/P&gt;&lt;P&gt;Regards Luca&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 15:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-image-not-booting/m-p/1386536#M184419</guid>
      <dc:creator>palu72</dc:creator>
      <dc:date>2021-12-14T15:28:08Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto project image not booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-image-not-booting/m-p/1386778#M184430</link>
      <description>&lt;P&gt;Hi Luca&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for sabrelite board one can look at boundary devices tutorial&lt;/P&gt;
&lt;P&gt;&lt;A href="https://boundarydevices.com/programming-emmc-on-i-mx6/" target="_blank"&gt;https://boundarydevices.com/programming-emmc-on-i-mx6/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 00:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-image-not-booting/m-p/1386778#M184430</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-12-15T00:37:22Z</dc:date>
    </item>
  </channel>
</rss>