<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8 QuadMax ISO7816 implementation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1385737#M184362</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a carrier board that contains an i.MX8 QuadMax processor.&lt;/P&gt;&lt;P&gt;I want to connect a SAM card slot to this processor but the manufacturer didn't make physical lines on the carrier board so a connection can be made between the SAM card and the integrated SIM module of the i.MX8 QuadMax (pins SIM0_CLK, SIM0_IO and so on).&lt;/P&gt;&lt;P&gt;Does anyone know how can I implement ISO 7816 communication with a running Linux OS on the i.MX8 processor without using the Linux drivers which use the SIM module?&lt;/P&gt;&lt;P&gt;I would appreciate any kind of help. Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Mon, 13 Dec 2021 15:25:33 GMT</pubDate>
    <dc:creator>Vlatakomarac</dc:creator>
    <dc:date>2021-12-13T15:25:33Z</dc:date>
    <item>
      <title>i.MX8 QuadMax ISO7816 implementation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1385737#M184362</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a carrier board that contains an i.MX8 QuadMax processor.&lt;/P&gt;&lt;P&gt;I want to connect a SAM card slot to this processor but the manufacturer didn't make physical lines on the carrier board so a connection can be made between the SAM card and the integrated SIM module of the i.MX8 QuadMax (pins SIM0_CLK, SIM0_IO and so on).&lt;/P&gt;&lt;P&gt;Does anyone know how can I implement ISO 7816 communication with a running Linux OS on the i.MX8 processor without using the Linux drivers which use the SIM module?&lt;/P&gt;&lt;P&gt;I would appreciate any kind of help. Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 15:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1385737#M184362</guid>
      <dc:creator>Vlatakomarac</dc:creator>
      <dc:date>2021-12-13T15:25:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 QuadMax ISO7816 implementation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1385894#M184373</link>
      <description>&lt;P&gt;Hi Nikola&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;how can I implement ISO 7816 communication with a running Linux OS on the&lt;/P&gt;
&lt;P&gt;&amp;gt;i.MX8 processor without using the Linux drivers which use the SIM module?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am afraid this is not possible, sorry. In general one can try simple sim unit test&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_sim_test?h=lf-5.10.52_2.1.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_sim_test?h=lf-5.10.52_2.1.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 23:09:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1385894#M184373</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-12-13T23:09:43Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 QuadMax ISO7816 implementation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1387291#M184503</link>
      <description>&lt;P&gt;Thank you Igor on your reply.&lt;/P&gt;&lt;P&gt;It is good to know if it is feasible or not so thank you.&lt;/P&gt;&lt;P&gt;What did you mean by using the sim unit test? What would be the goal of running this test?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 12:14:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1387291#M184503</guid>
      <dc:creator>Vlatakomarac</dc:creator>
      <dc:date>2021-12-15T12:14:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 QuadMax ISO7816 implementation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1387294#M184505</link>
      <description>&lt;P&gt;&amp;gt;What would be the goal of running this test?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;test basic sim functionality.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 12:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1387294#M184505</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-12-15T12:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 QuadMax ISO7816 implementation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1388075#M184568</link>
      <description>&lt;P&gt;I have been looking for a solution to the problem.&lt;/P&gt;&lt;P&gt;The only solution that I see is to use another microcontroller from the PN7462 family. They have integrated ISO UART modules, but this complicates the design because now there is another uC to program.&lt;/P&gt;&lt;P&gt;Could you recommend another IC that possibly implements ISO 7816 protocol but doesn't need to be programmed? I would use a TDA8037 but it requires that the uC implements the ISO 7816.&lt;/P&gt;&lt;P&gt;Thank you again. Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 10:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadMax-ISO7816-implementation/m-p/1388075#M184568</guid>
      <dc:creator>Vlatakomarac</dc:creator>
      <dc:date>2021-12-16T10:34:40Z</dc:date>
    </item>
  </channel>
</rss>